How to build core-image-rt on imx6qpsabresd

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to build core-image-rt on imx6qpsabresd

1,289 Views
enriqueencarnac
Contributor II

Hi,

I am trying to build “core-image-rt” for a imx6qpsabresd board using bitbake, but I am getting a message Nothing PROVIDES   ‘linux-yocto-rt’

I have included the PREFERRED_PROVIDER_virtual/kernel = “linux-yocto-rt” in my local.conf file, is that correct?

Or should I be somehow using linux-fslc-mx6-rt  somewhere?

Could you point me to some documentation/examples that build systems using pthreads and timers?

Labels (1)
0 Kudos
Reply
1 Reply

1,046 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Enrique Encarnación,

You are not specifying which BSP you are using but the problem in this case may be that while core-image-rt is available as part of the Open Embedded and thus is a valid image name, the i.MX6QP BSP does not support Linux Real Time. You would need to add the required dependencies and adjustments in order to build a Linux Real Time image for the i.MX6QP.

Regards,

0 Kudos
Reply