How to build a ramdisk (rootfs.ext2.gz.uboot) in yocto

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to build a ramdisk (rootfs.ext2.gz.uboot) in yocto

跳至解决方案
24,654 次查看
manjunathjoshi
Contributor V

Hello All,

I know the procedure to build ramdisk in ltib set up but wanted to try similar thing in yocto. Does anybody know how to build ramdisk?

Regards,

Manju

标签 (3)
1 解答
16,440 次查看
manjunathjoshi
Contributor V

Hello All,

I guess i have found out a way. Now yocto is not supporting .u-boot format for filesystem compilation.

The yocto now is supporting following image fstypes by default.

jffs2

  jffs2.sum

  cramfs

  ext2

  ext2.gz

  ext2.bz2

  ext3

  ext3.gz

  ext2.lzma

  btrfs

  live

  squashfs

  squashfs-xz

  ubi

  ubifs

  tar

  tar.gz

  tar.bz2

  tar.xz

  cpio

  cpio.gz

  cpio.xz

  cpio.lzma

  vmdk

  elf

So what i did was,

1. First i compiled with option ext3 and ext3.gz in local.conf.

IMAGE_FSTYPES += "ext3 ext3.gz "

Then, i used below command to get what i wanted.

2. Do bitbake again.

   bitbake core-image-minimal   // Now the image is of ext3.gz format

3. Now

   cd tmp/deploy/images/imx6qsabresd/

4. Run the below command to generate ramdisk image.

   mkimage -A arm -O linux -T ramdisk -C gzip -n core-image-minimal -d core-image-minimal-imx6qsabresd-XXXX.rootfs.ext3.gz core-image-minimal-imx6qsabresd-XXXXX.rootfs.ext3.gz.u-boot

Here core-image-minimal is the name of the RAMDISK image.

NOTE: MAKE SURE "mkimage" is there on UBUNTU else run

  sudo apt-get install u-boot-tools

To burn ramdisk

dd if=ramdiskimageXXX.uboot of=/dev/mmcblk0 bs=10M seek=1

Bootargs to boot from RAMDISK

U-Boot > setenv bootargs 'root=/dev/ram rw ramdisk_size=13239 console=ttymxc0,115200'

U-Boot > setenv bootcmd 'mmc dev 1;fatload mmc 1 0x12000000 uImage;fatload mmc 1 0x18000000 imx6q-magik2.dtb; mmc read 0x20000000 0x5000 0x2200;bootm 0x12000000 0x20000000 0x18000000'

U-Boot > boot

Thanks all,

在原帖中查看解决方案

6 回复数
16,440 次查看
jeremythien
Contributor I

This may be a bit late to be helpful, but I found I can accomplish this by adding these two lines to my image configuration:

inherit image_types_uboot

IMAGE_FSTYPES = "ext3.gz.u-boot"

P.S. I am using "morty".

0 项奖励
回复
16,440 次查看
manjunathjoshi
Contributor V

Hello Jeremy,

Thanks for the reply. But where exactly should i add this?

If i try to add it to core-image-minimal.bb file i get error like below,

ERROR: Unbuildable tasks were found.
These are usually caused by circular dependencies and any circular dependency chains found will be printed below. Increase the debug level to see a list of unbuildable tasks.

Please attach the .bb file

Regards,

Manju

0 项奖励
回复
16,441 次查看
manjunathjoshi
Contributor V

Hello All,

I guess i have found out a way. Now yocto is not supporting .u-boot format for filesystem compilation.

The yocto now is supporting following image fstypes by default.

jffs2

  jffs2.sum

  cramfs

  ext2

  ext2.gz

  ext2.bz2

  ext3

  ext3.gz

  ext2.lzma

  btrfs

  live

  squashfs

  squashfs-xz

  ubi

  ubifs

  tar

  tar.gz

  tar.bz2

  tar.xz

  cpio

  cpio.gz

  cpio.xz

  cpio.lzma

  vmdk

  elf

So what i did was,

1. First i compiled with option ext3 and ext3.gz in local.conf.

IMAGE_FSTYPES += "ext3 ext3.gz "

Then, i used below command to get what i wanted.

2. Do bitbake again.

   bitbake core-image-minimal   // Now the image is of ext3.gz format

3. Now

   cd tmp/deploy/images/imx6qsabresd/

4. Run the below command to generate ramdisk image.

   mkimage -A arm -O linux -T ramdisk -C gzip -n core-image-minimal -d core-image-minimal-imx6qsabresd-XXXX.rootfs.ext3.gz core-image-minimal-imx6qsabresd-XXXXX.rootfs.ext3.gz.u-boot

Here core-image-minimal is the name of the RAMDISK image.

NOTE: MAKE SURE "mkimage" is there on UBUNTU else run

  sudo apt-get install u-boot-tools

To burn ramdisk

dd if=ramdiskimageXXX.uboot of=/dev/mmcblk0 bs=10M seek=1

Bootargs to boot from RAMDISK

U-Boot > setenv bootargs 'root=/dev/ram rw ramdisk_size=13239 console=ttymxc0,115200'

U-Boot > setenv bootcmd 'mmc dev 1;fatload mmc 1 0x12000000 uImage;fatload mmc 1 0x18000000 imx6q-magik2.dtb; mmc read 0x20000000 0x5000 0x2200;bootm 0x12000000 0x20000000 0x18000000'

U-Boot > boot

Thanks all,

16,432 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Manjunath

for building manufacturing tool image one can look

at attached Yocto Guide sect.6.2 Manufacturing Tool, MFGTool

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

16,432 次查看
manjunathjoshi
Contributor V

Hello Igor,

Thanks for the immediate reply but i need a RAMDISK filesystem for a normal image like fsl-image-fb, or fsl-image-multimedia or even core-image-minimal is fine.

Regards,

Manju

0 项奖励
回复
16,432 次查看
manjunathjoshi
Contributor V

Hello All,

I don't know why this thread is assumed answered. The fact of the matter is, It is still not answered. Is there any way to build rootfs.ext3.gz and rootfs.ext3.gz.u-boot .

Do i need to build with specific options in conf/local.conf or the .bb file or the ./poky/meta/classes/image_types.bbclass.

If there is a way please anybody let me know.

Or give me a link where i can get this info.

Regards,

Manju

0 项奖励
回复