Hi,
There should be three things I need to build: rootfs, kernel, and uboot.
I downloaded kernel from here: linux-2.6-imx.git - Freescale i.MX Linux Tree, and uboot from here: uboot-imx.git - Freescale i.MX u-boot Tree. But I couldn't find where to download rootfs. Could somebody help?
With the cross-compiler installed previously, I built kernel by doing this under the root folder:
exportPATH=/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/:$PATHexport ARCH=armexport CROSS_COMPILE=arm-none-linux-gnueabi-make imx_v7_defconfigsudo apt-get install lzop (need to install zlop)make uImage LOADADDR=0x70008000 (need to specify load address to avoid build error)The output file uImage was put under ./arch/arm/boot.
I then tried to build uboot. The first three steps are the same as above. But at step 4, I couldn't find a config file in the whole uboot tree. Can somebody tell me how to build?
I used this as reference: Linux booting on IMX6 SABRESDB. I tried to follow Ed's notes, but when building uboot, I also couldn't find the config file.
Thanks a lot.
Jason
- For U-boot
make mrproper
make mx6qsabresd_config
make
Then flash it into the SD card: dd if=u-boot.imx of=/dev/mmcblk0 bs=512 seek=2; sync
- For kernel
make imx_v7_defconfig
make -j4 uImage LOADADDR=0x10008000
make imx6q-sabresd.dtb
(Your LOADADDR was incorrect).
- For rootfs
You can use your favourite rootfs (Yocto, LTIB, buldroot, etc). Yocto does all the above steps for you and generate you a sdcard image ready to boot.
Regards,
Fabio Estevam
Fabio,
Thanks to your reply, I was able to build u-boot.
I chose buildroot to build rootfs. I got the latest one from http://www.buildroot.org/download.html. I tried to build it in the following way:
$ make menuconfig...
# Target ARM (Little-Endian)
# Target Cortex A-9
# Under toolchain:
# External
# Sourcery Codebench ARM 2013.05
# Downloaded and installed
# Under System Configuration, chose ttymxc0 as the Port to run a getty (login prompt) on,
# Under Target Packages->Filesystem and Flash utilities: enable dosfstools and e2fsprogs
# Under Filesystem Images, selected Output cpio - gzipped; tar the root filesystem
$ make busybox-menuconfig...
# Do nothing, just exit (this step probably isn't necessary).
$ make V=1 2>&1 | tee make.out
But at the end, I got link error: "/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/../lib/gcc/arm-fsl-linux-gnueabi/4.6.2/../../../../arm-fsl-linux-gnueabi/bin/ld: cannot find crti.o: No such file or directory". I googled around for the whole day and just couldn't figure out the solution. Could you help please?
Thank you so much!
Jason
Hi Fabio,
To this point, I was able to build u-boot and kernel successfully. But after I flashed them to SD card, it won't boot (cannot even see u-boot prompt). I replaced u-boot on the SD card with the one I always used (3.0.35), then I could see u-boot prompt. But when it tried to load kernel from SD card, it failed on CRC check as below.
MX6Q SABRESD U-Boot > boot
mmc2 is current device
MMC read: dev # 2, block # 2048, count 8192 ... 8192 blocks read: OK
## Booting kernel from Legacy Image at 10800000 ...
Image Name: Linux-3.10.17
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 5201152 Bytes = 5 MB
Load Address: 10008000
Entry Point: 10008000
Verifying Checksum ... Bad Data CRC
ERROR: can't get kernel image!
BTW, I used the following commands to program u-boot and kernel onto SD card:
sudo dd if=u-boot-mx6q-sabresd.bin of=/dev/sde bs=512 seek=2 skip=2 conv=fsync
sudo dd if=uImage of=/dev/sde bs=512 seek=2048 conv=fsync
Do you have any idea what's going on?
Thank you very much.
Jason
Recent U-boot versions are flashed like this:
dd if=u-boot.imx of=/dev/mmcblk0 bs=512 seek=2; sync
Regards,
Fabio Estevam
Great. I used your command to flash U-boot and it can boot to the prompt now. Sorry I missed your first note about this command.
I then flashed the kernel to the card using the command "dd if=uImage of=/dev/sde bs=512 seek=2048; sync". I tweaked the boot env a little (attached at the end), but still got the same error.
U-Boot > boot
mmc1 is current device
MMC read: dev # 1, block # 2048, count 8192 ... 8192 blocks read: OK
## Booting kernel from Legacy Image at 12000000 ...
Image Name: Linux-3.10.17
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 5201152 Bytes = 5 MiB
Load Address: 10008000
Entry Point: 10008000
Verifying Checksum ... Bad Data CRC
ERROR: can't get kernel image!
U-Boot >
The boot envs are:
U-Boot > printenv
baudrate=115200
boot_fdt=try
bootargs=console=ttymxc0,115200 root=/dev/mmcblk1p1 rootwait
bootargs_base=setenv bootargs console=ttymxc0,115200
bootargs_mmc=setenv bootargs ${bootargs} root=/dev/mmcblk1p1 rootwait
bootcmd=run bootcmd_mmc
bootcmd_mfg=run mfgtool_args;bootm ${loadaddr} ${initrd_addr} ${fdt_addr};
bootcmd_mmc=run bootargs_base bootargs_mmc; mmc dev 1; mmc read ${loadaddr} 0x800 0x2000; bootm
bootdelay=1
bootfile=imx6q-sabresd.dtb
bootscript=echo Running bootscript from mmc ...; source
console=ttymxc0
ethact=FEC
ethaddr=00:04:9f:02:6e:c4
ethprime=FEC
fdt_addr=0x18000000
fdt_file=imx6q-sabresd.dtb
fdt_high=0xffffffff
get_cmd=dhcp
initrd_addr=0x12C00000
initrd_high=0xffffffff
ip_dyn=yes
loadaddr=0x12000000
loadbootscript=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${script};
loadfdt=fatload mmc ${mmcdev}:${mmcpart} ${fdt_addr} ${fdt_file}
loaduimage=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${uimage}
mfgtool_args=setenv bootargs console=ttymxc0,115200 rdinit=/linuxrc g_mass_storage.stall=0 g_mass_storage.removable=1 g_mass_storage.idVendor=0x066F g_mass_storage.idProduct=0x37FF g_mass_storage.iSerialNumber="" enable_wait_mode=off
mmcargs=setenv bootargs console=${console},${baudrate} ${smp} root=${mmcroot}
mmcboot=echo Booting from mmc ...; run mmcargs; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if run loadfdt; then bootm ${loadaddr} - ${fdt_addr}; else if test ${boot_fdt} = try; then bootm; else echo WARN: Cannot load the DT; fi; fi; else bootm; fi;
mmcdev=1
mmcpart=1
mmcroot=/dev/mmcblk0p2 rootwait rw
netargs=setenv bootargs console=${console},${baudrate} ${smp} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp
netboot=echo Booting from net ...; run netargs; if test ${ip_dyn} = yes; then setenv get_cmd dhcp; else setenv get_cmd tftp; fi; ${get_cmd} ${uimage}; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if ${get_cmd} ${fdt_addr} ${fdt_file}; then bootm ${loadaddr} - ${fdt_addr}; else if test ${boot_fdt} = try; then bootm; else echo WARN: Cannot load the DT; fi; fi; else bootm; fi;
script=boot.scr
uimage=uImage
video=mxcfb0:dev=hdmi,1920x1200M@60,if=RGB24
Environment size: 2221/8188 bytes
U-Boot >
Is there anything wrong somewhere?
Thanks,
Jason
Hi Jason
I pasted of a simple guide of booting up dtb and kernel from SD/MMC, you can refer to it and have a try:
supposed uImage is flashed to 2M offset of SD, and dtb is flashed to 1M offset of SD.
Boot kernel:
My kernel command line is “setenv bootargs console=ttymxc0,115200n8 noinitrd no_console_suspend root=/dev/mmcblk0p1 rw rootwait;mmc dev 0;mmc read 14000000 800 800;mmc read 10800000 1000 8000;bootm ${loadaddr} - ${dtbaddr}”
Hi Yongcai,
Your answer reminded me that I'm missing the .dtb file. My previous working u-boot/kernel didn't need it (maybe hardcoded everything), but this new u-boot/kernel DO need. After I built the .dtb file, I was able to boot.
Thank you so much.
Jason
Hi, Jason
Great, then can you help close this topic? Thanks!
I would suggest to strictly follow the instructions Ed provided here: Linux booting on IMX6 SABRESDB. It IS really working.
I didn't follow all of it the first time by skipping the dtb part, mainly because I didn't think it was necessary, since the Linux images 3.0.35 from Freescale didn't use .dtb files. Seems they hard-coded everything.
Thanks,
Jason
Jason
Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.
Thanks,
Yixing
Actually it was not directly solved. But I got an new image from Freescale field engineer, so I stopped trying any more.
Thanks.
Jason
Jason
We are closing the DI now. If you still need help, please feel free to reply with an update to this discussion.
Thanks,
Yixing
Jason
Thanks you for your reply. As you got new image, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.
Thanks,
Yixing
If you want to boot up L3.10.17 kernel, dtb is necessary, there is no hard coding device info for kernel.
Hi Yongcai,
Thank you for the reply.
When I built u-boot and kernel, seems the dtb files were not built automatically. In my kernel, I found these dts files. Should I pick one of them (like imx6q-sabresd.dts) and build into .dtb file? If so, could you suggest how? I googled around and found "In a normal flow, the DTS file is edited and compiled into a DTB file using a special compiler which comes with the Linux kernel sources" from here: A Tutorial on the Device Tree (Zynq) -- Part I | xillybus.com. I'm confused what special compiler it is.
./arch/arm/boot/dts/imx6q-sabresd-hdcp.dts
./arch/arm/boot/dts/imx6sl-evk-ldo.dts
./arch/arm/boot/dts/imx6dl-sabreauto.dts
./arch/arm/boot/dts/imx6dl-sabresd.dts
./arch/arm/boot/dts/imx6sl-evk-csi.dts
./arch/arm/boot/dts/imx6dl-sabresd-ldo.dts
./arch/arm/boot/dts/imx6dl-sabresd-hdcp.dts
./arch/arm/boot/dts/imx6q-sabrelite.dts
./arch/arm/boot/dts/imx6q-sabresd.dts
./arch/arm/boot/dts/imx6dl-sabreauto-ecspi.dts
./arch/arm/boot/dts/imx6dl-wandboard.dts
./arch/arm/boot/dts/imx6q-sabresd-ldo.dts
./arch/arm/boot/dts/imx6q-sabreauto.dts
./arch/arm/boot/dts/imx6q-sabreauto-flexcan1.dts
./arch/arm/boot/dts/imx6dl-sabreauto-flexcan1.dts
./arch/arm/boot/dts/imx6q-sbc6x.dts
./arch/arm/boot/dts/imx6q-sabreauto-gpmi-weim.dts
./arch/arm/boot/dts/imx6q-sabreauto-ecspi.dts
./arch/arm/boot/dts/imx6dl-sabreauto-gpmi-weim.dts
./arch/arm/boot/dts/imx6q-arm2.dts
./arch/arm/boot/dts/imx6sl-evk.dts
Another question is: do I really need a .dtb file to boot? I didn't have it when booting with Linux 3.0.35 from Freescale.
In order to exclude other factors (SD card programming, etc.) and only to test kernel, I actually tried one more thing, which is to boot kernel from network. Here is the details:
But the kernel hung at the very beginning:
U-Boot > tftp uImage_3.10.17
Using FEC device
TFTP from server 10.0.0.7; our IP address is 10.0.0.11
Filename 'uImage_3.10.17'.
Load address: 0x12000000
Loading: #################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#########################################
1.1 MiB/s
done
Bytes transferred = 5201216 (4f5d40 hex)
U-Boot > bootm
## Booting kernel from Legacy Image at 12000000 ...
Image Name: Linux-3.10.17
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 5201152 Bytes = 5 MiB
Load Address: 10008000
Entry Point: 10008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
No gpc device node -9, force to ldo-enable.
Starting kernel ...
I also downloaded the latest Yocto kernel source code (ver 3.10.3) from linux-yocto-3.10 - Linux 3.10 Embedded Kernel, built and tried to boot from network, and got the exact same symptom. I'm wondering if there's anything wrong in my build process. This is how I built it (I mentioned previously, and I was able to build u-boot with the same process (with different defconfig of course):
Could you comment?
Thanks a lot,
Jason
Hi Jason,
Sorry, but I have no experience with buildroot.
I would suggest you to send an email to the buildroot mailing list.
Regards,
Fabio Estevam