How to build Image for MarS Board i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to build Image for MarS Board i.MX6

3,898 Views
jerry-wang
Contributor I

Hello everyone:

I have a development board call marsboard by Embest with imx6 dual core chip.

These day I use the yocto to build the Image but there are no machin-Image support for MarS Board when use command "bitbake xxx-image".

Also,the viv GPU driver  had to include,does any document or website can reference?





0 Kudos
Reply
5 Replies

1,890 Views
frankba
Contributor III

Hi jerry,

here is an additional yocto layer for supporting MarS Board: FrankBau/meta-marsboard-bsp · GitHub

Frank

0 Kudos
Reply

1,890 Views
igorpadykov
NXP Employee
NXP Employee

Hi jerry

recently this board configuration was included in yocto, check

below yocto mailing list patch

Freescale OpenEmbedded/Yocto Layers discussion list ()

I would suggest to post this to meta-fsl-arm mailing list, so that someone familiar with this

board could try to assist you.

https://lists.yoctoproject.org/listinfo/meta-freescale

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,890 Views
benycx
Contributor I

Hi Igor,

Thanks for your answer. Excuse me if I am too much of a newbie to the subject but I don't find the trace of a "board configuration included in Yocto" at the link you provided, are you sure this was included in Yocto because I can't seem to find any trace of it. Thanks a lot in advance.

Kind regards

Ben

0 Kudos
Reply

1,890 Views
igorpadykov
NXP Employee
NXP Employee

Hi Benoit

suggest to check it in meta-fsl-arm mailing list

actually here we support only Freescale reference boards.

Best regards

igor

0 Kudos
Reply

1,890 Views
benycx
Contributor I

OK thanks!

0 Kudos
Reply