How to boot rom a SD card with U-BOOt

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to boot rom a SD card with U-BOOt

1,822件の閲覧回数
Jean-PaulLePape
Contributor I

Hello,

 I have an i.MX28 EVK board and used the script mk_mx28_sd to load uboot (ixm28_ivt_uboot.sb) on the SD card. The SD card is loaded on the second partition.

 The File system is loaded on the third partition.

I would like to know how can I configure UBOOT to be able to boot the kernel from the SD card. perhaps i nee to change the partition on the SD card?

By default UBOOT will try to find and boot the kernel from the network.

Thanks for your help,

:-)

タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,616件の閲覧回数
Jean-PaulLePape
Contributor I

Hi William,

 Thanks for your help. But I was able to pass this issue. I did rebuild imx28_ivt_uboot.sb and build a new kernel (3.2.1) and having that working.

Take care,

:-)

0 件の賞賛
返信

1,616件の閲覧回数
WilliamHuang
NXP Employee
NXP Employee

Hi

root@william-desktop:~# fdisk -u /dev/sdb

 

Command (m for help): n

Command action

   e   extended

   p   primary partition (1-4)

p

Partition number (1-4): 1

First sector (62-7744511, default 62): 16384

Last sector, +sectors or +size{K,M,G} (16384-7744511, default 7744511): 1064960

 

Command (m for help): n

Command action

   e   extended

   p   primary partition (1-4)

p

Partition number (1-4): 2

First sector (62-7744511, default 62): 1064961

Last sector, +sectors or +size{K,M,G} (1064961-7744511, default 7744511): 1081345

 

Command (m for help): n

Command action

   e   extended

   p   primary partition (1-4)

p

Partition number (1-4): 3

First sector (62-7744511, default 62): 1081346

Last sector, +sectors or +size{K,M,G} (1081346-7744511, default 7744511):

Using default value 7744511

 

Command (m for help): t

Partition number (1-4): 2

Hex code (type L to list codes): 53

Changed system type of partition 2 to 53 (OnTrack DM6 Aux3)

 

Command (m for help): w

The partition table has been altered!

 

Calling ioctl() to re-read partition table.

Syncing disks.

 

 

 

 

time sudo ./sdimage -f ./imx28_ivt_uboot.sb -d /dev/sdb

time sudo dd if=./uImage of=/dev/sdb bs=512 seek=256 conv=sync,notrunc

time sudo dd if=./rootfs.ext2 of=/dev/sdb3 bs=2048;sync

 

MX28 U-Boot > run bootcmd_mmc

The default uboot ENV parameter is included in u-boot and you could type the printenv to see it.

0 件の賞賛
返信