How to boot i.MX8M Mini using ECSPI Nor Flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to boot i.MX8M Mini using ECSPI Nor Flash

961 Views
Hariharan1
Contributor III

Hi expert,

We plan to boot from spi nor flash via ECSPI2 on iMx8 mini and do some research from community.

The following information is collected :

https://community.nxp.com/t5/i-MX-Processors/Boot-from-SPI-NOR-on-iMX-8M-Mini/m-p/1046463

https://community.nxp.com/t5/i-MX-Processors/Boot-iMX-8M-mini-LPDDR4-via-flash-conencted-to-ECSPI2/m...

Here has some question need you to provide more information:

1. Should spi nor bootloader can be use the same binary with SD card interface?

    If don't, how to generate a bootloader form spi nor flash via ecspi boot.

2. How to use uuu to burn this bootloader to spi nor? Should example_spinor.uuu can be use directly?

3. How to set boot switch for SPI Boot mode

Labels (1)
0 Kudos
Reply
0 Replies