How to boot Linux directly from UUU

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to boot Linux directly from UUU

ソリューションへジャンプ
2,187件の閲覧回数
Ryo_Aoki
Contributor III

Hi community.

I am currently using an i.MX6 SabreAI board.
I want to boot linux directly from serial downloader mode without writing to emmc or QSPI or SD card.
Is such usage possible?

 

I have already checked the following documents, but I do not understand the procedure.
whether it can be used in such a way
If possible, could you please tell me the command procedure?

 UUU (Universal Update Utility)Document (uuu.pdf)
 https://github.com/nxp-imx/mfgtools
 LF5.15.71.2.2.0のLinuxUserGuide

ラベル(1)
0 件の賞賛
返信
1 解決策
2,173件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信
2 返答(返信)
2,174件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

i.mx6 can boot up from usb, you can refer to the old community link

"https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Booting-Linux-through-USB-on-the-i-MX6-s..."

 

0 件の賞賛
返信
2,098件の閲覧回数
Ryo_Aoki
Contributor III

thank you for your reply. I will check the docs and give it a try.

0 件の賞賛
返信