Hi, I want to use asrc on imx6ul evk board using linux. I got a sample driver code from net. Every things works fine till the line below
if ((err = ioctl(fd_asrc, ASRC_CONVERT, &buf_info)) < 0)
My buf_info structure variable is correct with proper input and output buffer lengths, as well as input and output buffer pointers(they are not null). But still I am getting the following error in the teraterm..
| #define ASRC_CONVERT | _IOW(ASRC_IOC_MAGIC, 3, struct asrc_convert_buffer) |
error log:
root@linaro-ubuntu-desktop:~# fsl-asrc 2034000.asrc: invalid ioctl cmd!
Unable to handle kernel NULL pointer dereference at virtual address 00000000
pgd = 849b4000
[00000000] *pgd=89b50831, *pte=00000000, *ppte=00000000
Internal error: Oops: 817 [#3] PREEMPT SMP ARM
Modules linked in:
CPU: 0 PID: 2064 Comm: atc_sr_hw.elf Tainted: G D 3.14.38-6UL_ga+ge4944a5 #1
task: 85356400 ti: 87aa2000 task.ti: 87aa2000
PC is at __memzero+0x24/0x80
LR is at 0x0
pc : [<8028f6e4>] lr : [<00000000>] psr: 20000013
sp : 87aa3e44 ip : 00000000 fp : 8412fb00
r10: 00000000 r9 : 8412fb00 r8 : 00000000
r7 : 8412fb00 r6 : 87aa3ee0 r5 : 00000000 r4 : 894735c0
r3 : 00000000 r2 : 00000000 r1 : 0002ffc0 r0 : 00000000
Flags: nzCv IRQs on FIQs on Mode SVC_32 ISA ARM Segment user
Control: 10c53c7d Table: 849b406a DAC: 00000015
Process atc_sr_hw.elf (pid: 2064, stack limit = 0x87aa2238)
Stack: (0x87aa3e44 to 0x87aa4000)
3e40: 80585294 00000002 00000010 883ba600 88351a10 00000000 00000000
3e60: 00000000 00000000 883ba600 894735c0 00000004 00000040 894735c0 00200000
3e80: 894735c0 8071deec 883ba600 803609dc 00000008 88351a10 00000060 80584d30
3ea0: 00000004 00000000 00000000 88351a10 7eaba5b8 88351a10 87aa2000 00000000
3ec0: 894735c0 80586e7c 87aa3ee0 87aa2008 00000000 8071deec 89c43e88 8030f0a8
3ee0: 76c31008 769b2008 00001000 00001178 7eaba5e4 80071ff4 855116c8 00000002
3f00: 00000011 8847d600 00000002 8834e648 7eaba5b8 88a7ca80 40104303 00000003
3f20: 87aa2000 00000000 7eaba5e4 800e9dd8 00000000 00000000 00000000 00000000
3f40: 81c8fe3c 855116c0 00000011 86d91dc0 00000002 855116c8 87aa2000 00000000
3f60: 7eaba5e4 800da1c4 00000000 88a7ca80 7eaba5b8 88a7ca80 40104303 00000003
3f80: 87aa2000 00000000 7eaba5e4 800e9fcc 00000000 7eaba648 0000870c 00000036
3fa0: 8000e5e4 8000e460 00000000 7eaba648 00000003 40104303 7eaba5b8 7eaba5b8
3fc0: 00000000 7eaba648 0000870c 00000036 00000000 00000000 76f61000 7eaba5e4
3fe0: 00012ba4 7eaba5ac 00008e74 76eca92c 20000010 00000003 00378c00 00358d00
Code: e52de004 e1a0c002 e1a0e002 e2511040 (a8a0500c)
---[ end trace 5b7b3d0bf550318b ]---
Can some one please let me know how to resolve this problem. Thanks in advance..
Solved! Go to Solution.
Finally, it has got solved. The problem is due to incompatible mxc_asrc.h file. I was using wrong file.
Finally, it has got solved. The problem is due to incompatible mxc_asrc.h file. I was using wrong file.
Hi,
Thanks for sharing your solution. It will be very helpful.
Best Regards,
Alejandro