How to avoid V-Sync tearing i.MX 8M Mini with GStreamer, Qt?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to avoid V-Sync tearing i.MX 8M Mini with GStreamer, Qt?

2,004件の閲覧回数
VincasD
Contributor III

Hi,

I've attached video on how this GStreamer pipeline reproduces V-Sync tearing:

gst-launch-1.0 -v videotestsrc pattern=blink ! video/x-raw,width=1280,height=800 ! autovideosink

Originally I've discovered tearing in Qt 5.15-based QML application, where video is displayed using qmlglsink. we see diagonal tearing in fixed position on top of the screen.

Using fbdevsink in provided pipeline example makes it a bit "better" - the tear is no longer diagonal, just horizontal, but it still exists. But I can't use fbdevsink anyway as video must be composited inside Qt-based interface via qmlglsink...

I've tried various Qt eglfs-related environment variables, but nothing seems to help.

/etc/kms.conf in that device is:

# cat /etc/kms.conf  
{
 "device": "/dev/dri/card1",
 "hwcursor": true,
 "pbuffers": true,
 "outputs": [
   {
     "name": "DP",
     "mode": "1280x800"
   }
 ]
}

uname -a:

Linux imx8mmevk 5.10.72-lts-5.10.y+gb5085fe8a3ce #1 SMP PREEMPT Tue Oct 25 12:05:04 UTC 2022 aarch64 aarch64 aarch64 GNU/Linux

0 件の賞賛
返信
2 返答(返信)

1,984件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

You are using a kernel that is not supported, try to run the kernel 5.15.71 with qt6 this should works.

regards

0 件の賞賛
返信

1,968件の閲覧回数
VincasD
Contributor III
Thanks for your reply.

Do you mean that it ONLY works in Qt6? Not in Qt5?

What about using just GStreamer using pipeline I've provided? Should vsync issues dissapear with 5.15.71 kernel with GStreamer too?

Thanks!
0 件の賞賛
返信