How to adjust Rset and Rload value at i.MX51 TV Encoder output 1.6V level

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to adjust Rset and Rload value at i.MX51 TV Encoder output 1.6V level

ソリューションへジャンプ
1,721件の閲覧回数
andychien
Contributor III

Dear Sir,

Our customer want to adjust Rset and Rload value to meet TV output level 1.6V.

Could you help check how adjust  Rset and Rload value.

Thanks a lot,

We found Table 82 on i.MX6CEC.pdf Rev.6 10/2012

chapter 4.7.8.6.1 TV Encoder Performance Specification

Rset = 1.05 kΩ ±1%, resistor on VREFOUT pin to Ground

Rload = 37.5 Ω ±1%, output load to Ground

Full scale output voltage type=1.35V  and MAX=1.45V

ラベル(1)
0 件の賞賛
返信
1 解決策
1,668件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Andy

this module is characterized only under conditions

given in Table 82 of Datasheet. So other output voltages are not guaranteed.

Sorry, seems one needs to add some external circuits for boosting output

voltage.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,669件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Andy

this module is characterized only under conditions

given in Table 82 of Datasheet. So other output voltages are not guaranteed.

Sorry, seems one needs to add some external circuits for boosting output

voltage.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信