How to adjust Rset and Rload value at i.MX51 TV Encoder output 1.6V level

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to adjust Rset and Rload value at i.MX51 TV Encoder output 1.6V level

跳至解决方案
1,740 次查看
andychien
Contributor III

Dear Sir,

Our customer want to adjust Rset and Rload value to meet TV output level 1.6V.

Could you help check how adjust  Rset and Rload value.

Thanks a lot,

We found Table 82 on i.MX6CEC.pdf Rev.6 10/2012

chapter 4.7.8.6.1 TV Encoder Performance Specification

Rset = 1.05 kΩ ±1%, resistor on VREFOUT pin to Ground

Rload = 37.5 Ω ±1%, output load to Ground

Full scale output voltage type=1.35V  and MAX=1.45V

标签 (1)
0 项奖励
回复
1 解答
1,687 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Andy

this module is characterized only under conditions

given in Table 82 of Datasheet. So other output voltages are not guaranteed.

Sorry, seems one needs to add some external circuits for boosting output

voltage.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,688 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Andy

this module is characterized only under conditions

given in Table 82 of Datasheet. So other output voltages are not guaranteed.

Sorry, seems one needs to add some external circuits for boosting output

voltage.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复