How to add more FLAG of reason cause reboot with watchdog in Linux ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to add more FLAG of reason cause reboot with watchdog in Linux ?

Jump to solution
3,680 Views
toanjunifer
Senior Contributor I

Hi,

I'm using iMX8MM with Yocto. I'm trying to figure out the reason cause reboot with Watchdog. 

I find out watchdog.h and there are a lot of FLAGs: 

#define WDIOF_OVERHEAT 0x0001 /* Reset due to CPU overheat */
#define WDIOF_FANFAULT 0x0002 /* Fan failed */
#define WDIOF_EXTERN1 0x0004 /* External relay 1 */
#define WDIOF_EXTERN2 0x0008 /* External relay 2 */
#define WDIOF_POWERUNDER 0x0010 /* Power bad/power fault */
#define WDIOF_CARDRESET 0x0020 /* Card previously reset the CPU */
#define WDIOF_POWEROVER 0x0040 /* Power over voltage */
#define WDIOF_SETTIMEOUT 0x0080 /* Set timeout (in seconds) */
#define WDIOF_MAGICCLOSE 0x0100 /* Supports magic close char */
#define WDIOF_PRETIMEOUT 0x0200 /* Pretimeout (in seconds), get/set */
#define WDIOF_KEEPALIVEPING 0x8000 /* Keep alive ping reply */

But when I check with command, I get only 4 FLAG:

$ wdctl

Device: /dev/watchdog
Identity: imx2+ watchdog [version 0]
Timeout: 60 seconds
Pre-timeout: 0 seconds
FLAG                                DESCRIPTION                          STATUS           BOOT-STATUS
KEEPALIVEPING             Keep alive ping reply                     1                            0
MAGICCLOSE                  Supports magic close char           0                             0
PRETIMEOUT                  Pretimeout (in seconds)                0                             0
SETTIMEOUT                   Set timeout (in seconds)               0                            0

How do I get more of FLAG to use ?

Thank you so much,

Toan

Labels (1)
1 Solution
3,575 Views
toanjunifer
Senior Contributor I

After all, I have been added successfully. The last step is edit in menuconfig. 

Good luck and have a nice day.

Toan

View solution in original post

0 Kudos
Reply
3 Replies
3,576 Views
toanjunifer
Senior Contributor I

After all, I have been added successfully. The last step is edit in menuconfig. 

Good luck and have a nice day.

Toan

0 Kudos
Reply
3,575 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

 

You may find the driver here:

https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/watchdog/imx2_wdt.c?h=imx_4.14.98_...

 

Documentation for this driver is found here:

https://source.codeaurora.org/external/imx/linux-imx/tree/Documentation/watchdog?h=imx_4.14.98_2.0.0...

 

Also, I believe this commit will serve as a good example for what you're trying to achieve:

https://source.codeaurora.org/external/imx/linux-imx/commit/drivers/watchdog/imx2_wdt.c?h=imx_4.14.9...

 

Hope this helps,

Best regards,

Aldo.

3,575 Views
toanjunifer
Senior Contributor I

Hi nxf46838,

I actually edited driver file imx2_wdt.c. Then I execute bitbake command again. But it's not effective. 

This is my driver file after edited:

/*
* Watchdog driver for IMX2 and later processors
*
* Copyright (C) 2010 Wolfram Sang, Pengutronix e.K. <w.sang@pengutronix.de>
* Copyright (C) 2014 Freescale Semiconductor, Inc.
*
* some parts adapted by similar drivers from Darius Augulis and Vladimir
* Zapolskiy, additional improvements by Wim Van Sebroeck.
*
* This program is free software; you can redistribute it and/or modify it
* under the terms of the GNU General Public License version 2 as published by
* the Free Software Foundation.
*
* NOTE: MX1 has a slightly different Watchdog than MX2 and later:
*
* MX1: MX2+:
* ---- -----
* Registers: 32-bit 16-bit
* Stopable timer: Yes No
* Need to enable clk: No Yes
* Halt on suspend: Manual Can be automatic
*/

#include <linux/clk.h>
#include <linux/delay.h>
#include <linux/init.h>
#include <linux/interrupt.h>
#include <linux/io.h>
#include <linux/kernel.h>
#include <linux/module.h>
#include <linux/moduleparam.h>
#include <linux/of_address.h>
#include <linux/platform_device.h>
#include <linux/regmap.h>
#include <linux/watchdog.h>

#define DRIVER_NAME "imx2-wdt"

#define IMX2_WDT_WCR 0x00 /* Control Register */
#define IMX2_WDT_WCR_WT (0xFF << 8) /* -> Watchdog Timeout Field */
#define IMX2_WDT_WCR_WDA BIT(5) /* -> External Reset WDOG_B */
#define IMX2_WDT_WCR_SRS BIT(4) /* -> Software Reset Signal */
#define IMX2_WDT_WCR_WRE BIT(3) /* -> WDOG Reset Enable */
#define IMX2_WDT_WCR_WDE BIT(2) /* -> Watchdog Enable */
#define IMX2_WDT_WCR_WDZST BIT(0) /* -> Watchdog timer Suspend */

#define IMX2_WDT_WSR 0x02 /* Service Register */
#define IMX2_WDT_SEQ1 0x5555 /* -> service sequence 1 */
#define IMX2_WDT_SEQ2 0xAAAA /* -> service sequence 2 */

#define IMX2_WDT_WRSR 0x04 /* Reset Status Register */
#define IMX2_WDT_WRSR_TOUT BIT(1) /* -> Reset due to Timeout */

#define IMX2_WDT_WICR 0x06 /* Interrupt Control Register */
#define IMX2_WDT_WICR_WIE BIT(15) /* -> Interrupt Enable */
#define IMX2_WDT_WICR_WTIS BIT(14) /* -> Interrupt Status */
#define IMX2_WDT_WICR_WICT 0xFF /* -> Interrupt Count Timeout */

#define IMX2_WDT_WMCR 0x08 /* Misc Register */

#define IMX2_WDT_MAX_TIME 128
#define IMX2_WDT_DEFAULT_TIME 60 /* in seconds */

#define WDOG_SEC_TO_COUNT(s) ((s * 2 - 1) << 8)

struct imx2_wdt_device {
   struct clk *clk;
   struct regmap *regmap;
   struct watchdog_device wdog;
   bool ext_reset;
};

static bool nowayout = WATCHDOG_NOWAYOUT;
module_param(nowayout, bool, 0);
MODULE_PARM_DESC(nowayout, "Watchdog cannot be stopped once started (default="
__MODULE_STRING(WATCHDOG_NOWAYOUT) ")");


static unsigned timeout = IMX2_WDT_DEFAULT_TIME;
module_param(timeout, uint, 0);
MODULE_PARM_DESC(timeout, "Watchdog timeout in seconds (default="
__MODULE_STRING(IMX2_WDT_DEFAULT_TIME) ")");

static const struct watchdog_info imx2_wdt_info = {
                     .identity = "imx2+ CheckPoint watchdog",
                     .options = WDIOF_KEEPALIVEPING |
                     WDIOF_SETTIMEOUT |
                     WDIOF_MAGICCLOSE |
                     WDIOF_OVERHEAT |
                     WDIOF_FANFAULT |
                     WDIOF_EXTERN1 |
                     WDIOF_EXTERN2 |
                     WDIOF_POWERUNDER |
                     WDIOF_CARDRESET |
                     WDIOF_POWEROVER |
                     WDIOF_PRETIMEOUT,
};

static const struct watchdog_info imx2_wdt_pretimeout_info = {
.identity = "imx2+ CheckPoint watchdog",
.options = WDIOF_KEEPALIVEPING |
WDIOF_SETTIMEOUT |
WDIOF_MAGICCLOSE |
WDIOF_OVERHEAT |
WDIOF_FANFAULT |
WDIOF_EXTERN1 |
WDIOF_EXTERN2 |
WDIOF_POWERUNDER |
WDIOF_CARDRESET |
WDIOF_POWEROVER |
WDIOF_PRETIMEOUT,
};

static int imx2_wdt_ping(struct watchdog_device *wdog);
static inline bool imx2_wdt_is_running(struct imx2_wdt_device *wdev);

static int imx2_wdt_restart(struct watchdog_device *wdog, unsigned long action,
void *data)
{
struct imx2_wdt_device *wdev = watchdog_get_drvdata(wdog);
unsigned int wcr_enable = IMX2_WDT_WCR_WDE;

/* Use internal reset or external - not both */
if (wdev->ext_reset)
wcr_enable |= IMX2_WDT_WCR_SRS; /* do not assert int reset */
else
wcr_enable |= IMX2_WDT_WCR_WDA; /* do not assert ext-reset */

/* Assert SRS signal */
regmap_write(wdev->regmap, IMX2_WDT_WCR, wcr_enable);

if (imx2_wdt_is_running(wdev))
imx2_wdt_ping(wdog);

/*
* Due to imx6q errata ERR004346 (WDOG: WDOG SRS bit requires to be
* written twice), we add another two writes to ensure there must be at
* least two writes happen in the same one 32kHz clock period. We save
* the target check here, since the writes shouldn't be a huge burden
* for other platforms.
*/
regmap_write(wdev->regmap, IMX2_WDT_WCR, wcr_enable);
regmap_write(wdev->regmap, IMX2_WDT_WCR, wcr_enable);

/* wait for reset to assert... */
mdelay(100);
dev_err(wdog->parent, "failed to assert %s reset, trying with timeout\n",
wdev->ext_reset ? "external" : "internal");

return 0;
}

static inline void imx2_wdt_setup(struct watchdog_device *wdog)
{
struct imx2_wdt_device *wdev = watchdog_get_drvdata(wdog);
u32 val;

regmap_read(wdev->regmap, IMX2_WDT_WCR, &val);

/* Suspend timer in low power mode, write once-only */
val |= IMX2_WDT_WCR_WDZST;
/* Strip the old watchdog Time-Out value */
val &= ~IMX2_WDT_WCR_WT;
/* Generate internal chip-level reset if WDOG times out */
if (!wdev->ext_reset)
val &= ~IMX2_WDT_WCR_WRE;
/* Or if external-reset assert WDOG_B reset only on time-out */
else
val |= IMX2_WDT_WCR_WRE;
/* Keep Watchdog Disabled */
val &= ~IMX2_WDT_WCR_WDE;
/* Set the watchdog's Time-Out value */
val |= WDOG_SEC_TO_COUNT(wdog->timeout);

regmap_write(wdev->regmap, IMX2_WDT_WCR, val);

/* enable the watchdog */
val |= IMX2_WDT_WCR_WDE;
regmap_write(wdev->regmap, IMX2_WDT_WCR, val);
}

static inline bool imx2_wdt_is_running(struct imx2_wdt_device *wdev)
{
u32 val;

regmap_read(wdev->regmap, IMX2_WDT_WCR, &val);

return val & IMX2_WDT_WCR_WDE;
}

static int imx2_wdt_ping(struct watchdog_device *wdog)
{
struct imx2_wdt_device *wdev = watchdog_get_drvdata(wdog);

regmap_write(wdev->regmap, IMX2_WDT_WSR, IMX2_WDT_SEQ1);
regmap_write(wdev->regmap, IMX2_WDT_WSR, IMX2_WDT_SEQ2);
return 0;
}

static void __imx2_wdt_set_timeout(struct watchdog_device *wdog,
unsigned int new_timeout)
{
struct imx2_wdt_device *wdev = watchdog_get_drvdata(wdog);

regmap_update_bits(wdev->regmap, IMX2_WDT_WCR, IMX2_WDT_WCR_WT,
WDOG_SEC_TO_COUNT(new_timeout));
}

static int imx2_wdt_set_timeout(struct watchdog_device *wdog,
unsigned int new_timeout)
{
__imx2_wdt_set_timeout(wdog, new_timeout);

wdog->timeout = new_timeout;
return 0;
}

static int imx2_wdt_set_pretimeout(struct watchdog_device *wdog,
unsigned int new_pretimeout)
{
struct imx2_wdt_device *wdev = watchdog_get_drvdata(wdog);

if (new_pretimeout >= IMX2_WDT_MAX_TIME)
return -EINVAL;

wdog->pretimeout = new_pretimeout;

regmap_update_bits(wdev->regmap, IMX2_WDT_WICR,
IMX2_WDT_WICR_WIE | IMX2_WDT_WICR_WICT,
IMX2_WDT_WICR_WIE | (new_pretimeout << 1));
return 0;
}

static irqreturn_t imx2_wdt_isr(int irq, void *wdog_arg)
{
struct watchdog_device *wdog = wdog_arg;
struct imx2_wdt_device *wdev = watchdog_get_drvdata(wdog);

regmap_write_bits(wdev->regmap, IMX2_WDT_WICR,
IMX2_WDT_WICR_WTIS, IMX2_WDT_WICR_WTIS);

watchdog_notify_pretimeout(wdog);

return IRQ_HANDLED;
}

static int imx2_wdt_start(struct watchdog_device *wdog)
{
struct imx2_wdt_device *wdev = watchdog_get_drvdata(wdog);

if (imx2_wdt_is_running(wdev))
imx2_wdt_set_timeout(wdog, wdog->timeout);
else
imx2_wdt_setup(wdog);

set_bit(WDOG_HW_RUNNING, &wdog->status);

return imx2_wdt_ping(wdog);
}

static const struct watchdog_ops imx2_wdt_ops = {
.owner = THIS_MODULE,
.start = imx2_wdt_start,
.ping = imx2_wdt_ping,
.set_timeout = imx2_wdt_set_timeout,
.set_pretimeout = imx2_wdt_set_pretimeout,
.restart = imx2_wdt_restart,
};

static const struct regmap_config imx2_wdt_regmap_config = {
.reg_bits = 16,
.reg_stride = 2,
.val_bits = 16,
.max_register = 0x8,
};

static int __init imx2_wdt_probe(struct platform_device *pdev)
{
struct imx2_wdt_device *wdev;
struct watchdog_device *wdog;
struct resource *res;
void __iomem *base;
int ret;
u32 val;

wdev = devm_kzalloc(&pdev->dev, sizeof(*wdev), GFP_KERNEL);
if (!wdev)
return -ENOMEM;

res = platform_get_resource(pdev, IORESOURCE_MEM, 0);
base = devm_ioremap_resource(&pdev->dev, res);
if (IS_ERR(base))
return PTR_ERR(base);

wdev->regmap = devm_regmap_init_mmio_clk(&pdev->dev, NULL, base,
&imx2_wdt_regmap_config);
if (IS_ERR(wdev->regmap)) {
dev_err(&pdev->dev, "regmap init failed\n");
return PTR_ERR(wdev->regmap);
}

wdev->clk = devm_clk_get(&pdev->dev, NULL);
if (IS_ERR(wdev->clk)) {
dev_err(&pdev->dev, "can't get Watchdog clock\n");
return PTR_ERR(wdev->clk);
}

wdog = &wdev->wdog;
wdog->info = &imx2_wdt_info;
wdog->ops = &imx2_wdt_ops;
wdog->min_timeout = 1;
wdog->max_hw_heartbeat_ms = IMX2_WDT_MAX_TIME * 1000;
wdog->parent = &pdev->dev;

ret = platform_get_irq(pdev, 0);
if (ret > 0)
if (!devm_request_irq(&pdev->dev, ret, imx2_wdt_isr, 0,
dev_name(&pdev->dev), wdog))
wdog->info = &imx2_wdt_pretimeout_info;

ret = clk_prepare_enable(wdev->clk);
if (ret)
return ret;

regmap_read(wdev->regmap, IMX2_WDT_WRSR, &val);
wdog->bootstatus = val & IMX2_WDT_WRSR_TOUT ? WDIOF_CARDRESET : 0;

wdev->ext_reset = of_property_read_bool(pdev->dev.of_node,
"fsl,ext-reset-output");
wdog->timeout = clamp_t(unsigned, timeout, 1, IMX2_WDT_MAX_TIME);
if (wdog->timeout != timeout)
dev_warn(&pdev->dev, "Initial timeout out of range! Clamped from %u to %u\n",
timeout, wdog->timeout);

platform_set_drvdata(pdev, wdog);
watchdog_set_drvdata(wdog, wdev);
watchdog_set_nowayout(wdog, nowayout);
watchdog_set_restart_priority(wdog, 128);
watchdog_init_timeout(wdog, timeout, &pdev->dev);

if (imx2_wdt_is_running(wdev)) {
imx2_wdt_set_timeout(wdog, wdog->timeout);
set_bit(WDOG_HW_RUNNING, &wdog->status);
}

/*
* Disable the watchdog power down counter at boot. Otherwise the power
* down counter will pull down the #WDOG interrupt line for one clock
* cycle.
*/
regmap_write(wdev->regmap, IMX2_WDT_WMCR, 0);

ret = watchdog_register_device(wdog);
if (ret) {
dev_err(&pdev->dev, "cannot register watchdog device\n");
goto disable_clk;
}

dev_info(&pdev->dev, "timeout %d sec (nowayout=%d)\n",
wdog->timeout, nowayout);

return 0;

disable_clk:
clk_disable_unprepare(wdev->clk);
return ret;
}

static int __exit imx2_wdt_remove(struct platform_device *pdev)
{
struct watchdog_device *wdog = platform_get_drvdata(pdev);
struct imx2_wdt_device *wdev = watchdog_get_drvdata(wdog);

watchdog_unregister_device(wdog);

if (imx2_wdt_is_running(wdev)) {
imx2_wdt_ping(wdog);
dev_crit(&pdev->dev, "Device removed: Expect reboot!\n");
}
return 0;
}

static void imx2_wdt_shutdown(struct platform_device *pdev)
{
struct watchdog_device *wdog = platform_get_drvdata(pdev);
struct imx2_wdt_device *wdev = watchdog_get_drvdata(wdog);

if (imx2_wdt_is_running(wdev)) {
/*
* We are running, configure max timeout before reboot
* will take place.
*/
imx2_wdt_set_timeout(wdog, IMX2_WDT_MAX_TIME);
imx2_wdt_ping(wdog);
dev_crit(&pdev->dev, "Device shutdown: Expect reboot!\n");
}
}

#ifdef CONFIG_PM_SLEEP
/* Disable watchdog if it is active or non-active but still running */
static int imx2_wdt_suspend(struct device *dev)
{
struct watchdog_device *wdog = dev_get_drvdata(dev);
struct imx2_wdt_device *wdev = watchdog_get_drvdata(wdog);

/* The watchdog IP block is running */
if (imx2_wdt_is_running(wdev)) {
/*
* Don't update wdog->timeout, we'll restore the current value
* during resume.
*/
__imx2_wdt_set_timeout(wdog, IMX2_WDT_MAX_TIME);
imx2_wdt_ping(wdog);
}

clk_disable_unprepare(wdev->clk);

return 0;
}

/* Enable watchdog and configure it if necessary */
static int imx2_wdt_resume(struct device *dev)
{
struct watchdog_device *wdog = dev_get_drvdata(dev);
struct imx2_wdt_device *wdev = watchdog_get_drvdata(wdog);
int ret;

ret = clk_prepare_enable(wdev->clk);
if (ret)
return ret;

if (watchdog_active(wdog) && !imx2_wdt_is_running(wdev)) {
/*
* If the watchdog is still active and resumes
* from deep sleep state, need to restart the
* watchdog again.
*/
imx2_wdt_setup(wdog);
}
if (imx2_wdt_is_running(wdev)) {
imx2_wdt_set_timeout(wdog, wdog->timeout);
imx2_wdt_ping(wdog);
}

return 0;
}
#endif

static SIMPLE_DEV_PM_OPS(imx2_wdt_pm_ops, imx2_wdt_suspend,
imx2_wdt_resume);

static const struct of_device_id imx2_wdt_dt_ids[] = {
{ .compatible = "fsl,imx21-wdt", },
{ /* sentinel */ }
};
MODULE_DEVICE_TABLE(of, imx2_wdt_dt_ids);

static struct platform_driver imx2_wdt_driver = {
.remove = __exit_p(imx2_wdt_remove),
.shutdown = imx2_wdt_shutdown,
.driver = {
.name = DRIVER_NAME,
.pm = &imx2_wdt_pm_ops,
.of_match_table = imx2_wdt_dt_ids,
},
};

module_platform_driver_probe(imx2_wdt_driver, imx2_wdt_probe);

MODULE_AUTHOR("Wolfram Sang");
MODULE_DESCRIPTION("Watchdog driver for IMX2 and later");
MODULE_LICENSE("GPL v2");
MODULE_ALIAS("platform:" DRIVER_NAME);

nxf46838 wrote:

Hello,

 

You may find the driver here:

https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/watchdog/imx2_wdt.c?h=imx_4.14.98_...

 

Documentation for this driver is found here:

https://source.codeaurora.org/external/imx/linux-imx/tree/Documentation/watchdog?h=imx_4.14.98_2.0.0...

 

Also, I believe this commit will serve as a good example for what you're trying to achieve:

https://source.codeaurora.org/external/imx/linux-imx/commit/drivers/watchdog/imx2_wdt.c?h=imx_4.14.9...

 

Hope this helps,

Best regards,

Aldo.

Then I execute:

 $ bitbake core-image-base

May you help me to make it right ?

Thank you so much,

Toan

0 Kudos
Reply