How to add kernel parameter?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to add kernel parameter?

ソリューションへジャンプ
10,227件の閲覧回数
nguyentuan_k58h
Contributor II

Hi experts,

I want to use the on-chip board Wifi QCA6174 of IMX8M Quad Evk Kit. I'm using yocto to build my distro fsl-imx-xwayland, kernel 4.9.88-2.0.0 (rocko)

Following release notes document "For i.MX 8MQuad, it needs to add kernel parameter
"pci=nomsi" to support Murata 1CQ Wi-Fi". But i didn't find the way to add it. 

Can you tell me how I can solve this problem and the steps for using the wlan chip QCA6174? Thank you.

Best regards,

1 解決策
6 返答(返信)
10,025件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Tuan

this is general linux parameter and one can try to use it in the same way as

described in Table 10. Common kernel boot parameters. QCA6174 is described in

sect.4.12 Wi-Fi QCA6174 Linux Manual in Linux 4.9.88_2.0.0 BSP & Multimedia Codecs Documentation

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

10,025件の閲覧回数
nguyentuan_k58h
Contributor II

Hi igor,

I still can not figure out how to add kernel parameter.

I have try modprobe kernel.pci=nomsi but it did not work.

Btw, where is QCA6174 driver located in /lib/firmware/.

0 件の賞賛
返信
10,026件の閲覧回数
igorpadykov
NXP Employee
NXP Employee
10,025件の閲覧回数
nguyentuan_k58h
Contributor II

Hi igorpadykov‌

I've tried your solution in version L5.4.3_1.0.0 . It did not work. the interface wlp1s0 was not shown.

I've read release note of this version, there no guide to enable onchip wifi.

Can you tell me how to enable onchip wifi in version L5.4.3_1.0.0?

0 件の賞賛
返信
10,025件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Tuan

one can try to follow sect.4.13.7 Configuring WLAN from User Space

Linux Manual included in Linux 5.4.3_1.0.0 Documentation

Best regards
igor

0 件の賞賛
返信
10,025件の閲覧回数
nguyentuan_k58h
Contributor II

Hi igorpadykov‌

Here is image which i flashed "https://www.nxp.com/webapp/Download?colCode=L5.4.3_1.0.0_MX8MQ&appType=license "

Actually, i've tried to procedure from "Reference manual" guide. 

When i run "wpa_supplicant -B -i wlp1s0 -c /etc/wpa_supplicant.conf -D nl80211"

Error show "Could not interface wlp1s0 flags: No such device" 

By the way, command "iw dev" show nothing when i hit. 

0 件の賞賛
返信