How to add imx8mp HDMI driver in uboot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to add imx8mp HDMI driver in uboot

1,651 Views
darshan_kukadiya
Contributor I

I have phycore-imx8m plus board, i have build uboot 20.04 stand alone.

so, How can i add or enable HDMI driver in u-boot?

0 Kudos
Reply
3 Replies

1,621 Views
brian14
NXP TechSupport
NXP TechSupport

Hi @darshan_kukadiya

Thank you for contacting NXP Support.

Based on the following thread that functionality is unsupported on the i.MX8MP.
Re: Support U-Boot splash screen to kernel in imx8MP for Linux NXP - NXP Community

Have a great day!

 

0 Kudos
Reply

1,301 Views
sunannan
Contributor II

@brian14 

 您好:

         imx8mp的uboot为什么不支持HDMI显示?我在尝试移植HDMI驱动,如果是cpu硬件导致无法在uboot阶段无法显示,能说明原因吗?我的需求是使用HDMI屏幕在3秒左右显示logo。

1,295 Views
darshan_kukadiya
Contributor I
exactly the same thing i wanted to do .want to show logo in boot time on HDMI display for imx8mp.
0 Kudos
Reply