I have phycore-imx8m plus board, i have build uboot 20.04 stand alone.
so, How can i add or enable HDMI driver in u-boot?
Hi @darshan_kukadiya,
Thank you for contacting NXP Support.
Based on the following thread that functionality is unsupported on the i.MX8MP. Re: Support U-Boot splash screen to kernel in imx8MP for Linux NXP - NXP Community
Have a great day!
@brian14
您好:
imx8mp的uboot为什么不支持HDMI显示?我在尝试移植HDMI驱动,如果是cpu硬件导致无法在uboot阶段无法显示,能说明原因吗?我的需求是使用HDMI屏幕在3秒左右显示logo。