How to add custom board entry in Android source code?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to add custom board entry in Android source code?

5,054 次查看
hrushinale
Contributor III

Hello Community,

  We are using a custom board running on i.MX6 solo.We have successfully ported the Embedded Linux on our board.

Now,we want to port the android .For that we followed the Android USers Guide but in that they mentioned the Image building procedure for development boards.

I want to build the Android Images for our custom borad but I don't know How to add our new boards entry in Android source code.

Kindly help me regarding this issue

Best Regards,

Hrushi

标记 (1)
3 回复数

4,167 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Hrushi,

    It is not difficult to add a new board to android source code if your board is based on i.MX6 evaluation board, I only give you general steps, see below:

asume your board's name is: MX6Q_MyBoard

(1)Creating directory For the board

Open "myandroid/device/fsl/", and create a directory named "MX6Q_MyBoard".

Create-name.png

(2)Copying all files in sabresd_6dq to the directory

If your board is based on sabread EVK, copy all file in sabresd_6dq to MX6Q_MyBoard

Copy-files.png

(3)Changing configurations in BoardConfig.mk to yours

Check the file carefully, and modify some contents, such as device/fsl/sabresd_6dq, it should be changed to device/fsl/MX6Q_MyBoad, TARGET_BOOTLOADER_BOARD_NAME := SABRESD to  TARGET_BOOTLOADER_BOARD_NAME := MyBoard, etc. That is to say, you should change all information on sabresd to be yours.

(4)Add your products to AndroidProducts.mk

Open device/fsl/imx6/AndroidProducts.mk, and add it in:

PRODUCT_MAKEFILES := \
  $(LOCAL_DIR)/evk_6sl.mk \
  $(LOCAL_DIR)/sabreauto_6q.mk \
  $(LOCAL_DIR)/sabresd_6dq.mk \
  $(LOCAL_DIR)/sabresd_6sx.mk \
  $(LOCAL_DIR)/sabreauto_6sx.mk \

$(LOCAL_DIR)/MX6Q_MyBoard.mk \

(5)Creating MX6Q_MyBoard.mk file in current directory

In device/fsl/imx6 path, create MX6Q_MyBoard.mk file, and copy all contents of sabresd_6dq.mk to it.

Then according to your schematic, adjust correcponding configurations, don't forget it.

(6)Adding your products to vendorsetup.sh

Open the file , and add 2 lines at the end:

......

add_lunch_combo MX6Q_MyBoard-eng
add_lunch_combo MX6Q_MyBoard-user

   OK, generally speaking, you need to do above 6 steps, then your products can be compiled independently, but don't forget to modify configurations to be in accord with your board.

  Hope these steps are helpful for you!

Best Regards,

Weidong

4,166 次查看
hrushinale
Contributor III

Hello Sir,

Thanks for your help.

I Added the Board entry as per the above post and I am getting the bootloader image and kernel image in my myandroid/out directory .

But I am not getting the recovery and system image .

Do I need to modify any other files apart from the above post like recovery folder etc.

Kindly guide me regarding this issue.

Thanks & Regards,

Hrushi

0 项奖励
回复

4,167 次查看
hrushinale
Contributor III

Thanks You So much for your Guidance.

0 项奖励
回复