How to add Watchdog in U-boot for 2014 version yocto source

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to add Watchdog in U-boot for 2014 version yocto source

5,500件の閲覧回数
bandarulavanya
Contributor V

Hi All,

I added watchdog timer in u boot like below .

in include/configs/imx6dl-sabresd.h

     #define CONFIG_IMX_CONFIG

in /board/freescale/imx6dl-sabresd/imx6dl-sabresd.c

int board_late_init(void)

{

        int ret = 0;

#ifdef CONFIG_CMD_BMODE

        add_board_boot_modes(board_boot_modes);

#endif

#ifdef CONFIG_SYS_I2C_MXC

        setup_i2c(1, CONFIG_SYS_I2C_SPEED,

                        0x7f, &i2c_pad_info1);

        ret = setup_pmic_voltages();

        if (ret)

                return -1;

#endif

#ifdef CONFIG_ENV_IS_IN_MMC

        board_late_mmc_env_init();

#endif

#ifdef CONFIG_IMX_WATCHDOG

        hw_watchdog_init();

#endif

        return 0;

}

like this.

If i stop in u-boot after my time out it is rebooting . if any crash occur in kernel in that time also it is rebooting.

But if file system is not mounted then it is not rebooting how can i achieve that.

and after enabling watchdog in u boot. my wdt_driver_test.out in unit-tests is not working.

unit-tests$ ./wdt_driver_test.out 10 5 0

Here after i given ctrl+c also it is not rebooting.

unit-tests$ ./wdt_driver_test.out 1 2 0

In this case also after 1 sec it should reboot but it is not.How can i solve this issue please if any one knows kindly suggest me.

Thanks & Regards,
Lavany

ラベル(3)
0 件の賞賛
返信
9 返答(返信)

4,278件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Lavany

seems you are using some customized uboot version,

could you try with nxp uboot-imx

uboot-imx.git - Freescale i.MX u-boot Tree

unit-tests are working properly with nxp linux&uboot.

Best regards

igor

0 件の賞賛
返信

4,278件の閲覧回数
bandarulavanya
Contributor V

Hi igorpadykov ,

Sorry , actually uboot version is 2014 not 2013 that i got from yocto setup.

Thanks

Lavanya

0 件の賞賛
返信

4,278件の閲覧回数
bandarulavanya
Contributor V

Hi igorpadykov ,
In my kernel dts file i have like this

&gpc {

        /* use ldo-bypass, u-boot will check it and configure */

        fsl,ldo-bypass = <0>;

        fsl,wdog-reset = <1>;

};

&wdog1 {

        status = "okay";

};

so now if i am running

./wdt_driver_test.out 10 5 0

Starting wdt_driver (timeout: 10, sleep: 5, test: ioctl)

Trying to set timeout value=10 seconds

The actual timeout was set to 10 seconds

Now reading back -- The timeout is 10 seconds

^C

Now exactly after 10 seconds it is rebooting.

In U-boot also i am trying to enable wdog.For that i did like below.

In board file i added like this in board_late_init function

#ifdef CONFIG_IMX_WATCHDOG

        hw_watchdog_init();

#endif

and in includes/configs/custom_board.h file   #define CONFIG_IMX_WATCHDOG 1

and i reduced time in drivers/watchdog/imx_watchdog.c

//#define CONFIG_WATCHDOG_TIMEOUT_MSECS 128000

#define CONFIG_WATCHDOG_TIMEOUT_MSECS 12000

after enabling wdt in u boot my kernel watchdog is not working what ever time i given , it is taking more than 5 mins to reboot.

and in log i observed like below after enabling watchdog in u boot

Starting udev

udevd[130]: starting version 182

bootlogd: cannot allocate pseudo tty: No such file or directory

random: dd urandom read with 95 bits of entropy available

ALSA: Restoring mixer settings...

/usr/sbin/alsactl: load_state:1729: No soundcards found...

Mon May 30 11:44:05 UTC 2016

random: nonblocking pool is initialized

INIT: Entering runlevel: 5

Configuring network interfaces... fec 2188000.ethernet eth0: no PHY, assuming direct connection to switch

libphy: PHY fixed-0:00 not found

fec 2188000.ethernet eth0: could not attach to PHY

ifconfig: SIOCSIFFLAGS: No such device

Starting Xserver

Starting system message bus: dbus.

Starting rpcbind daemon...done.

Starting advanced power management daemon: No APM support in kernel

(failed.)

Starting syslogd/klogd: done

* Starting Avahi mDNS/DNS-SD Daemon: avahi-daemon

   ...done.

Starting Telephony daemon

Starting Linux NFC daemon

Starting OProfileUI server

PU: Power-on latency exceeded, new value 4670334 ns {if watchdog is not enabled in u boot it is not coming}

How to solve this issue if any one knows kindly help me .

Thanks & Regards,

Lavanya

0 件の賞賛
返信

4,278件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Lavanya

wdog should not be enabled twice as some bits could

be written once. In general nxp has service helping with customization

NXP Professional Services:

http://www.nxp.com/support/nxp-professional-services:PROFESSIONAL-SERVICE

Pro-Support contact www.nxp.com/prosupport

Best regards

igor

0 件の賞賛
返信

4,278件の閲覧回数
bandarulavanya
Contributor V

Hi igorpadykov ,

i observed that i got random: nonblocking pool is initialized In this case watchdog is taking more than 5mins to reboot and some times not rebooting if it is not coming then wdt is working properly .

how to solve this error .

Thanks & Regards,

Lavanya

0 件の賞賛
返信

4,278件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Lavanya

also one can post that on uboot mail list

U-Boot Info Page

Best regards

igor

0 件の賞賛
返信

4,278件の閲覧回数
bandarulavanya
Contributor V

igorpadykov ,

But in 3.0.35 kernel watchdog is working properly i enabled both u boot and kernel .

but in yocto setup u boot with 2014 and kernel with 3.14.28 is giving problem

0 件の賞賛
返信

4,278件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Lavanya

in nxp uboot there is no ../imx6dl-sabresd/imx6dl-sabresd.c

could you try with nxp uboot-imx

Best regards

igor

0 件の賞賛
返信

4,278件の閲覧回数
bandarulavanya
Contributor V

Hi ,

mx6sabresd.h this is original file that is for my custom board .

mx6sabresd/mx6sabresd.c are correct names , i want why that u-boot watchdog is not releasing when i reach kernel.

Thanks & Regards,

Lavanya

0 件の賞賛
返信