Which PMIC is better for i.MX6UL: PF3000 or PF3001?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Which PMIC is better for i.MX6UL: PF3000 or PF3001?

1,977 次查看
maximpodberezni
Contributor III


Hi!

I'm making a design based on imx6 UltraLite processor and want to use a PMIC. I have a reference design based on PF3000 but have not a similar one based on PF3001. The PF3001 product page states "The PF3001 is ideally suited for i.MX6UL processors", but I can't find any reference schematics for this PMIC. I can see little differences between these ICs, but I know how difficult it can be to bring up custom boards and just don't want to have lots of hardware iterations and a headache in software side.

Please suggest the best PMIC for imx6UL processor without problems to bring up the board and accessible from distributors

标签 (2)
标记 (1)
0 项奖励
回复
3 回复数

1,399 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Maxim

PF3001 is simplified version of PF3000 and one can use both options.

For schematic please create service request.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,399 次查看
maximpodberezni
Contributor III

Hi Igor!

My distributor created the service request for SPF-28865, but it was for PF3000, not PF3001. Please suggest a number for the service request

0 项奖励
回复

1,399 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Maxim

SCH-29090

Best regards

igor

0 项奖励
回复