How to activate PCIe Data_Link_Layer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to activate PCIe Data_Link_Layer

2,184 Views
george
Senior Contributor II

Dear all,

We want to use PCIe on i.MX6.

The method of generate the Configuration Cycle is being known gradually.

Currently, the method of setting Data Link Layer to Active is investigated.

To this, I think that setting is required in an order from the physical layer.

Please recommend, if there are materials which are consulted.

And, which around in Source of Linux should be seen?

Best Regards,

George

Tags (3)
0 Kudos
Reply
2 Replies

1,980 Views
igorpadykov
NXP Employee
NXP Employee

Hi George, most suitable way to run SDK PCIe

example, please read included in package

iMX6_Firmware_Guide.pdf. Linux "L3.0.35_4.1.0_ER_SOURCE"

package can be found on the same link, in Linux package please read

i.MX_6Dual6Quad_Linux_Reference_Manual.pdf

"MX6_PLATFORM_SDK "

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&nodeId=018rH3ZrDRB24A&fpsp=1&t...

One can run tests from iRAM using scripts below

iRAM (OCRAM) i.MX6 SDK Application

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

1,980 Views
george
Senior Contributor II

Dear Chip,

I try to look for required information from the materials which you showed.

And it will post again here, when there is a question.

Thanks

Best Regards,

George

0 Kudos
Reply