MTBF value for PF0100 PMIC and I.MX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MTBF value for PF0100 PMIC and I.MX6

3,248件の閲覧回数
aneeshts
Contributor I

Hi All,

   Anybody can provide me Documents that specifies MTBF(Mean Time between failure) or FIT(Failure in time) value for the I.MX6 Quad, Dual,Solo, Dual lite and the PMIC PF0100?




Regards

Aneesh

ラベル(4)
0 件の賞賛
返信
1 返信

1,506件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

He, ANEESH

Freescale does not provide such documents. You

can refer to documents below, for MTBF values you can enter

ticket to Freescale support.

Application Note AN4725 Rev. 0, 05/2013

i.MX 6Solo/6DualLite Product Usage Lifetime Estimates

http://www.freescale.com/files/32bit/doc/app_note/AN4725.pdf

Application Note AN4724 (rev. 0, 04/2013)

"i.MX 6Dual/6Quad Product Usage Lifetime Estimates"

http://www.freescale.com/files/32bit/doc/app_note/AN4724.pdf

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信