How to Select The SION Bit in Different Conditions?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to Select The SION Bit in Different Conditions?

1,547件の閲覧回数
tony_l_cai
Contributor III

Hi,all

     Maybe I dont know how to use the SION Bit, could you tell me what conditons do we need to set SION bit? please give me an example,3Q~

ラベル(2)
0 件の賞賛
返信
1 返信

1,371件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi tony

SW Loopback (SION) – the SION bit (SW Input On in IOMUXC_SW_MUX_CTL)

override the regular PAD functionality and forces the input path to

be active regardless of the value driven by the corresponding

module. It can be used for:

Loop Back - Module X drives the PAD and also receive PAD value as an

input. Required by I2C,SDHC modules.

GPIO Capture - Module X drives the PAD and the value is captured by GPIO.

Loop Back to module Y - Module X drives the PAD and module Y also receives

PAD value as an input. This can be used for driving module Y input without

connecting a real device on board.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信