How to IMX28 device UART and SPI output voltage select?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to IMX28 device UART and SPI output voltage select?

1,256 Views
sung-ukjang
Contributor II

Dear Freescale.

I need to 1.8V out put USRT and SPI function on IMX28 board.

How to change output voltage on Linux source?

please help.

Thanks.

Labels (1)
0 Kudos
Reply
2 Replies

1,000 Views
Yuri
NXP Employee
NXP Employee

  Please use pin configuring in

<ltib_dir>/rpm/BUILD/linux/arch/arm/mach-mx28/ mx28evk.c

(parameter .voltage) which refer to C-function mxs_pin_voltage() in

<litb_dir>/rpm/BUILD/linux/arch/arm/mach-mx28/pinctrl.c


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,000 Views
sung-ukjang
Contributor II

Dear Freescale

I had change 1.8V output below signal pin.

SSP0_SCK, SSP0_CMD, SSP0_DATA0,
SSP0_DATA1, SSP0_DATA2, SSP0_DATA3,

ENET0_MDC, ENET0_MDIO,
ENET0_RXD0, ENET0_RXD1

But, not chaenged below signal 1.8V out put

AUART3_RX, AUART3_TX,
AUART3_CTS, AUART3_RTS

Do you know How to change UART3 function output voltage?

please help.

0 Kudos
Reply