How to Enabling FlexCAN in devicetree on iMX6 (Solidrun Hummingboard)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to Enabling FlexCAN in devicetree on iMX6 (Solidrun Hummingboard)

2,734 Views
johnwalkr
Contributor I

I'm trying to enable flexCAN bus 1 on the 26 pin GPIO header on the HomeRun Hummingboard. The iMX6 version is Core Solo, part number MCIMX6S5DVM10AB. I've confirmed that this chip has 2 flexCAN buses, and I've confirmed that they can be accessed on pin 16 and 18 of the GPIO header. The pins are SD3_CMD (can be muxed to CAN TX) and SD3_CLK (can be muxed to CAN RX).

I have 2 CAN transceivers I can use. Both are working on other devices (an SH2 microcontroller,  beaglebone black and raspberry pi) so I cam confident that they are set up correctly. The transceivers are TI SN65HVD1050 and Microchip MCP2551.

I'm using Yocto with kernel 3.14.14.

I changed 2 device tree dtsi files to enable CAN, according to this post and others:

https://community.freescale.com/thread/318776

After recompiling, I can send and recieve messages to and from the raspberry pi and beaglebone black, but on the same CAN netwwork, I can't send or recieve to/from the iMX6. I get an error in dmesg, leading me to believe that I have not set up device tree correctly:

dmesg | grep -i "can"

[    1.432240] vcan: Virtual CAN interface driver

[    1.436722] CAN device driver interface

[    1.440823] 2090000.flexcan supply xceiver not found, using dummy regulator

[    1.448778] flexcan 2090000.flexcan: device registered (reg_base=a0a18000, irq=142)

[    2.639349] can: controller area network core (rev 20120528 abi 9)

[    2.651219] can: raw protocol (rev 20120528)

[    2.655541] can: broadcast manager protocol (rev 20120528 t)

[    2.663294] can: netlink gateway (rev 20130117) max_hops=1

[    2.775105] md: Scanned 0 and added 0 devices.

I'm not really sure what my next step in troubleshooting is, aside from hoping someone else has overcome a similar problem and can offer advice.

Labels (3)
0 Kudos
Reply
2 Replies

1,256 Views
zhenli
Contributor II

Hi,

    I  have that issue  too!

      Do  you solve it now?Could you tell me?

Thank you very much!

0 Kudos
Reply

1,256 Views
BiyongSUN
NXP Employee
NXP Employee

kernel 3.14.14 is not freescale BSP release version.

Please use freescale official BSP release.

0 Kudos
Reply