How set mx6q_sabresd output the display data to YUV format

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How set mx6q_sabresd output the display data to YUV format

跳至解决方案
2,063 次查看
kaisun1
Contributor III

HI :

      we use ms6q_sabresd board as a platform to development .  we need the board output the display data  format is 20-bit YCbCr .

Then i read kernel and uboot code .and only find the code what is support HDMI LVDS and RGB  format . what i shoud do ?

Thanks anyway!

1 解答
1,862 次查看
ChucoChe
NXP Employee
NXP Employee

Please check the Linux Release notes table 6. the video section. If the format you want doesn't works in setting by kernel boot parameter. I'm afraid you will have to add it in the kernel or driver.

Michel

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,863 次查看
ChucoChe
NXP Employee
NXP Employee

Please check the Linux Release notes table 6. the video section. If the format you want doesn't works in setting by kernel boot parameter. I'm afraid you will have to add it in the kernel or driver.

Michel

0 项奖励
回复
1,862 次查看
kaisun1
Contributor III

Hi michel:

              this proble i have resolve. imx6 is support it .

1,862 次查看
kaisun1
Contributor III

HI ,This problem has been solved.   now  i  can output 720P video data.  but 720i  is not work.

0 项奖励
回复