How set mx6q_sabresd output the display data to YUV format

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How set mx6q_sabresd output the display data to YUV format

ソリューションへジャンプ
1,948件の閲覧回数
kaisun1
Contributor III

HI :

      we use ms6q_sabresd board as a platform to development .  we need the board output the display data  format is 20-bit YCbCr .

Then i read kernel and uboot code .and only find the code what is support HDMI LVDS and RGB  format . what i shoud do ?

Thanks anyway!

ラベル(6)
1 解決策
1,747件の閲覧回数
ChucoChe
NXP Employee
NXP Employee

Please check the Linux Release notes table 6. the video section. If the format you want doesn't works in setting by kernel boot parameter. I'm afraid you will have to add it in the kernel or driver.

Michel

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,748件の閲覧回数
ChucoChe
NXP Employee
NXP Employee

Please check the Linux Release notes table 6. the video section. If the format you want doesn't works in setting by kernel boot parameter. I'm afraid you will have to add it in the kernel or driver.

Michel

0 件の賞賛
返信
1,747件の閲覧回数
kaisun1
Contributor III

Hi michel:

              this proble i have resolve. imx6 is support it .

1,747件の閲覧回数
kaisun1
Contributor III

HI ,This problem has been solved.   now  i  can output 720P video data.  but 720i  is not work.

0 件の賞賛
返信