How repair SSI bitclock / frame sync fault

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How repair SSI bitclock / frame sync fault

1,909 次查看
rosciio
Contributor I

Hello

Im'working on imx6Q cpu with SSI audio interface. SSI1 works very well into playback and capture mode.

The problem is:

I would like to improve it. I notice that if have a fault on physical bitclock signal I have a problem. In particular in Network mode (with more then 1 slots) slot shift of 1 slot respect the frame sync. the same problem there isn't if I have a fault on frame sync signal.

I enable interrupts on SIER and I see into SISR RFS, TFS, RLS and TLS flags.

I would like to see 1 flag of RFS and after 1 flag og RLS. Flags showed randomic events.

I hope someone help me.

thanks 

Marco from Italy

标记 (5)
0 项奖励
回复
2 回复数

1,805 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Marco

once initialized, special sequence may be required for changing SSI parameters,

it is better described in older SSI documentation like

sect.56.5 Initialization/Application Information i.MX51 Reference Manual

https://www.nxp.com/docs/en/reference-manual/MCIMX51RM.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,805 次查看
rosciio
Contributor I

Hi Igorpadykov,

I will check the sequence.

thanks

Marco

0 项奖励
回复