How repair SSI bitclock / frame sync fault

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How repair SSI bitclock / frame sync fault

1,911件の閲覧回数
rosciio
Contributor I

Hello

Im'working on imx6Q cpu with SSI audio interface. SSI1 works very well into playback and capture mode.

The problem is:

I would like to improve it. I notice that if have a fault on physical bitclock signal I have a problem. In particular in Network mode (with more then 1 slots) slot shift of 1 slot respect the frame sync. the same problem there isn't if I have a fault on frame sync signal.

I enable interrupts on SIER and I see into SISR RFS, TFS, RLS and TLS flags.

I would like to see 1 flag of RFS and after 1 flag og RLS. Flags showed randomic events.

I hope someone help me.

thanks 

Marco from Italy

ラベル(6)
タグ(5)
0 件の賞賛
返信
2 返答(返信)

1,807件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Marco

once initialized, special sequence may be required for changing SSI parameters,

it is better described in older SSI documentation like

sect.56.5 Initialization/Application Information i.MX51 Reference Manual

https://www.nxp.com/docs/en/reference-manual/MCIMX51RM.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,807件の閲覧回数
rosciio
Contributor I

Hi Igorpadykov,

I will check the sequence.

thanks

Marco

0 件の賞賛
返信