How redirect console on USB port

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How redirect console on USB port

1,764 Views
v_pazienza
Contributor I

Hello,
we are working with a i.MX6ULL based board. We are using the debian distribution "Linux imx6ul-var-dart 4.9.88" customized by Variscite which is the owner of the module we are using.
We are now making some further customization to use the module in our equipment, succesfully.
We configured USB#2 as pheriperal with serial gadged enabled and we need to use it in order to redirect the console on.
Changing  U-Boot from uart1 to uart3 and the console parameter as ttymxc2 as reported on 
http://www.variwiki.com/index.php?title=DART-6UL_UART all works fine.
We set console parameter to ttyGS0 in order to redirect almost the kernel console, but the serial terminal on PC Host does not receive anything.

Thanks in advance.

Vincenzo Pazienza

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,661 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Vincenzo,

If you are using a Variscite board and their BSP, you may consider directly asking to Variscite on its support page about the customization that you would like to implement:

Variscite Support Center - Variscite 

Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

0 Kudos
Reply