i.MX 8M Mini Configuration Resistor Strength

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 8M Mini Configuration Resistor Strength

Jump to solution
3,177 Views
adevries
Contributor V

Hello Community,

For boot mode configuration pins on the 8M Mini like BOOT_MODE0, BOOT_MODE1, TEST_MODE, and JTAG_MOD, does it matter if I connect a very strong pull-up or pull-down resistor to these pins? Can I connect these pins directly to NVCC_JTAG or GND?

I believe these pins are always inputs, so I think it's acceptable to tie them directly to a power rail, but I want to ask and verify this before I accidentally blow up my 8M Mini.

Thanks

Labels (1)
0 Kudos
Reply
1 Solution
2,987 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

 

For this case scenario we suggest to place a switch, just like in our EVK, if you plan to change the logic state of the BOOT_MODE.

Also, the connection you mentioned shouldn't be done, you can use one of these two options for the BOOT_MODE pins:

  • Pulled up or down using the resistor I previously mentioned
  • Connected directly to NVCC_JTAG or GND

 

Pull-up regulate the amount of current it drives to the pin, if the power is not an issue it can be tied directly to VDD.

 

Hope this helps,

Best regards,

Aldo.

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

4 Replies
2,987 Views
adevries
Contributor V

Thanks Aldo, that's good to know!

0 Kudos
Reply
2,987 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

 

Usually for pull-up resistors any value between 4.7k ~ 10k ohms, 4.7k ohm is preferred in high noise environments, for pull downs usually a 100k ohm is recommended.

 

Hope this helps,

Best regards,

Aldo.

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
2,987 Views
adevries
Contributor V

Hi Aldo,

Thanks for the response. I know that the recommendation is for a 4.7-10k pull up and 100k pull down resistor. However, in my application, I'm looking to temporarily override some pull-up and pull-down resistors. For example, if I have BOOT_MODE1 set to 1 by pulling it high with 4.7k ohms, and I need to set BOOT_MODE1 to 0 temporarily, can I just ground the pin? 

What if BOOT_MODE0 was set to 0 by pulling it low with 100k ohms, and I need to set it to 1. Can I connect the pin to NVCC_JTAG?

Thanks

0 Kudos
Reply
2,988 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

 

For this case scenario we suggest to place a switch, just like in our EVK, if you plan to change the logic state of the BOOT_MODE.

Also, the connection you mentioned shouldn't be done, you can use one of these two options for the BOOT_MODE pins:

  • Pulled up or down using the resistor I previously mentioned
  • Connected directly to NVCC_JTAG or GND

 

Pull-up regulate the amount of current it drives to the pin, if the power is not an issue it can be tied directly to VDD.

 

Hope this helps,

Best regards,

Aldo.

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------