How read PCM data from BT?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How read PCM data from BT?

3,181 Views
younhawoo
Contributor I

Dear Freescale,

I tried reading PCM data from BT.

Please refer attachment schematic file.

CPU : i.mx6 dual

android : jellybean 4.3

kernel version : 3.0.35

I found imx-3stack-bt.c and blutooth.c from this community.

But, the files version is low(kernel 2.6 base).

The files dismatch my project.

Could you help me?

Thank you,

Labels (2)
0 Kudos
Reply
1 Reply

2,956 Views
art
NXP Employee
NXP Employee

There is the Linux 3.0.35 kernel BSP, available for download on the Freescale web site (check under the "Operating System Software-Board Support Packages" tab):

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&fpsp=1&tab=Design_Tools_Tab

It already contains the Bluetooth stack driver supporting the A2DP profile.

Please try it.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply