How "input clock" and "output clock" are used in i.MX6 ASRC?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How "input clock" and "output clock" are used in i.MX6 ASRC?

Jump to solution
2,059 Views
satoshishimoda
Senior Contributor I

Hi community,

Please see Figure 15-4 in IMX6SDLRM (Rev.1).

I want to know how "Input clock X" and "Output clock X" are used in i.MX6 ASRC.

I understand "Input clock X" are used for input of Pre-processing in Figure 15-3, and "Output clock X" are used for input of Post-processing in Figure 15-3 as attached image.

Is this correct?

If my understanding is wrong, could you let me know how these clocks are used?

Best Regards,

Satoshi Shimoda

Labels (4)
Tags (1)
0 Kudos
Reply
1 Solution
1,770 Views
Yuri
NXP Employee
NXP Employee

"Input clock X"  corresponds Fsin (Figure 15-3. Signal processing configurations of the i.MX6 SDL RM )

"Output clock X" corresponds Fsout.


Table 15-7 (Pre-processing, post-processing options) shows what configurations are possible when

it is needed to convert the sampling rate of a signal, associated with an input clock into a signal, associated

with a different output clock.

View solution in original post

0 Kudos
Reply
1 Reply
1,771 Views
Yuri
NXP Employee
NXP Employee

"Input clock X"  corresponds Fsin (Figure 15-3. Signal processing configurations of the i.MX6 SDL RM )

"Output clock X" corresponds Fsout.


Table 15-7 (Pre-processing, post-processing options) shows what configurations are possible when

it is needed to convert the sampling rate of a signal, associated with an input clock into a signal, associated

with a different output clock.

0 Kudos
Reply