How "input clock" and "output clock" are used in i.MX6 ASRC?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How "input clock" and "output clock" are used in i.MX6 ASRC?

跳至解决方案
2,091 次查看
satoshishimoda
Senior Contributor I

Hi community,

Please see Figure 15-4 in IMX6SDLRM (Rev.1).

I want to know how "Input clock X" and "Output clock X" are used in i.MX6 ASRC.

I understand "Input clock X" are used for input of Pre-processing in Figure 15-3, and "Output clock X" are used for input of Post-processing in Figure 15-3 as attached image.

Is this correct?

If my understanding is wrong, could you let me know how these clocks are used?

Best Regards,

Satoshi Shimoda

标签 (4)
标记 (1)
0 项奖励
回复
1 解答
1,802 次查看
Yuri
NXP Employee
NXP Employee

"Input clock X"  corresponds Fsin (Figure 15-3. Signal processing configurations of the i.MX6 SDL RM )

"Output clock X" corresponds Fsout.


Table 15-7 (Pre-processing, post-processing options) shows what configurations are possible when

it is needed to convert the sampling rate of a signal, associated with an input clock into a signal, associated

with a different output clock.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,803 次查看
Yuri
NXP Employee
NXP Employee

"Input clock X"  corresponds Fsin (Figure 15-3. Signal processing configurations of the i.MX6 SDL RM )

"Output clock X" corresponds Fsout.


Table 15-7 (Pre-processing, post-processing options) shows what configurations are possible when

it is needed to convert the sampling rate of a signal, associated with an input clock into a signal, associated

with a different output clock.

0 项奖励
回复