How much capacity of the SD-Card that the SABRE-SDP based on i.MX 6Quad support ? ( MCIMX6Q-SDP )

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How much capacity of the SD-Card that the SABRE-SDP based on i.MX 6Quad support ? ( MCIMX6Q-SDP )

1,361件の閲覧回数
patcharasirigul
Contributor II

Hello Everyone,

I would like to know how much capacity of the SD-Card that the SABRE-SDP based on i.MX 6Quad support. Because I would like to use the SABRE-SDP for recording video from the camera.

Thank you so much. :smileyhappy:

ラベル(2)
0 件の賞賛
返信
1 返信

1,058件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Patchara

please check below link (all are supported with i.MX6)

Capacity (SD/SDHC/SDXC) - SD Association

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信