How many USB ports can handle for iMAX6Q custom hardware ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How many USB ports can handle for iMAX6Q custom hardware ?

2,436 Views
peteramond
Contributor V

Dear All,

iMAX6 supports USB 2.0. How many USB 2.0 ports can handle iMAX6Q ? If I connect hub with USB interface are there any limitations for this ?

Regards.

Peter.

Labels (2)
3 Replies

2,314 Views
joanxie
NXP TechSupport
NXP TechSupport

refer to the Data sheet:

USB:
— One High Speed (HS) USB 2.0 OTG (Up to 480 Mbps), with integrated HS USB PHY
— Three USB 2.0 (480 Mbps) hosts:
– One HS host with integrated High Speed PHY
– Two HS hosts with integrated High Speed Inter-Chip (HS-IC) USB PHY

2,314 Views
peteramond
Contributor V

Hi Joan,

Thank you for your response.

I need to know how many devices can be used with "One HS host with integrated High Speed PHY" ? If I'm using USB hub. Can I connect 14 devices to usb hub via this host port of iMAX6. How it affect to the data speed and how can we understand its limitations.

Regards,

Peter.

0 Kudos
Reply

2,314 Views
joanxie
NXP TechSupport
NXP TechSupport

can't say how many ports hub imx6 can support, which depends on your hub, you can refer to the topic as below:

https://community.nxp.com/thread/359720 

0 Kudos
Reply