How many CSI-2(MIPI) cameras can be interfaced simultaniously in IMX6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How many CSI-2(MIPI) cameras can be interfaced simultaniously in IMX6

2,090 次查看
ashokp
Contributor I

Hi All,

Please let me know how many CSI-2(MIPI) cameras can be interfaced simultaniously in IMX6.

Thanks,

P.Ashok

标记 (3)
0 项奖励
回复
2 回复数

1,878 次查看
Yuri
NXP Employee
NXP Employee

Hello,

i.MX6 contains single MIPI CSI to IPU Gasket (CSI2IPU), so one camera can be connected

to it, but  MIPI CSI 2supports up to four concurrent (virtual) channels

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,878 次查看
kenyung
Contributor I

But there is only one clk lane, how can we seperate one clk lane to two? is there a ic to seperate the clk lane to two ?

0 项奖励
回复