How get QuadSPI configuration parameters for IMX6ULL-EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How get QuadSPI configuration parameters for IMX6ULL-EVK

1,169 Views
黎明周
Contributor I

Hello,everybody

   I have a IMX6ULL-EVK board, want to boot use QuadSPI.I have tried use imgutil tool get  sdk20-app.img in SDK_2.2_MCIM6ULL. reference below

QQ图片20181214101812.png

but can not boot from QSPI,the bin is make by IAR,what is wrong?

      run mfgtool2-sdk20-mx6ul-evk-qspi-nor-n25q256a.vbs ,like these status:

1.png

2.png

3.png4.png5.png

in the last picture,nothing occur forever.why the reminder is "No Device Connected",confirm the usb cabe is connect with board in this process? The  Getting Started with MCUXpresso SDK for i.MX 6ULL Derivatives.pdf is like this

6.png

      

      I see the sdk20-app.img ,it  file contain  IVT, boot data,dcd table ,etc.but didn't contain the boot device configuration parameters.

    I think the img not have device configuration parameters, so can't boot from QSPI,do you think?

   Read IMX6ULLRM.pdf, 

8.6.3 QuadSPI configuration parameters

 this is a table, 512 byte,how to make the table use tool? Is there such a tool?

Thanks.

Regards,

Liming.Zhou

Labels (1)
0 Kudos
Reply
1 Reply

1,012 Views
igorpadykov
NXP Employee
NXP Employee

Hi Liming

QuadSPI configuration parameters are provided in

mfg tool folder ..OS Firmware/files (its name like "qspi-nor-micron-n25q256a-config")

Mfg Tool can be found on link

i.MX Software|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------