How enable cache on PCIe in i.MX6?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How enable cache on PCIe in i.MX6?

2,114件の閲覧回数
massohy
Contributor II

Dear All,

 

I am using i.MX6 as PCIe RC. I will write data via PCIe to EP device by ARM CPU.

I want to write with as much as possible large TLP packet by ARM CPU in i.MX6, but I can only 8 byte with memcpy() in yocto linux.

I referred the community, I found that i.MX6 can write by 32 byte unit at PCIe cached.

 

I referred to patch code attached to https://community.nxp.com/docs/DOC-95014.

I thought it will be ok that I modify pci-imx6.c , but this patch had many different from my driver. And, I thought many codes of modification of its patch was for EP side.  

 

Please tell me, how can I enable cache on PCIe? If cache is enable, then can I write over 8 bytes unit TLP packet from ARM CPU in RC side i.MX6?

 

And, if I use PCIe with cached, is that system able to use stable?

 

Best Regards,

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,864件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi mas

below link provides solution for improving pcie performance using arm core (with cache enabled) or ipu

dma as masters for RC side. I am afraid there are no other ways to improve it.

i.MX6Q PCIe EP/RC Validation System 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信