How does i.MX535 handle jumbo frames

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How does i.MX535 handle jumbo frames

Jump to solution
2,605 Views
TerryMcHenry
Contributor II

The reference manual in not real clear on this topic.  Does anyone have more details on how to handle Jumbo Frames and what the limitations are?

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,460 Views
Yuri
NXP Employee
NXP Employee

The i.MX53 FEC supports the following :

If the transmit frame length exceeds MAX_FL bytes the BABT interrupt is

asserted: however, the entire frame is transmitted (no truncation).

  When the receive frame length exceeds MAX_FL bytes the BABR interrupt is generated,

and the LG bit in the end of frame RxBD is set. The frame is not truncated (unless the

frame length exceeds 2047 bytes).

   So, maximum length is 2047.

View solution in original post

0 Kudos
Reply
3 Replies
2,461 Views
Yuri
NXP Employee
NXP Employee

The i.MX53 FEC supports the following :

If the transmit frame length exceeds MAX_FL bytes the BABT interrupt is

asserted: however, the entire frame is transmitted (no truncation).

  When the receive frame length exceeds MAX_FL bytes the BABR interrupt is generated,

and the LG bit in the end of frame RxBD is set. The frame is not truncated (unless the

frame length exceeds 2047 bytes).

   So, maximum length is 2047.

0 Kudos
Reply
2,460 Views
TerryMcHenry
Contributor II

Thanks, Yuri.  I ran this question by FSL as well and their reply was similar, i.e. 2047 is the limit.

0 Kudos
Reply
2,460 Views
jamesbone
NXP TechSupport
NXP TechSupport

Besides the Reference Manual, I can olny said that you can take a look to the Linux  ENET driver of the i.Mx53. but I do not think we have more information besides that.

0 Kudos
Reply