How do you get HDMI output to show in portrait instead of landscape?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How do you get HDMI output to show in portrait instead of landscape?

6,726件の閲覧回数
alexanderchung
Contributor II

When HDMI video output is used, Android always displays in landscape mode. How can I get it to show up in portrait mode instead? Is there somewhere in the kernel source I can modify to accomplish this? Or perhaps a setting that needs to be changed?

i.MX6Q SabreAuto

Android 4.3 image

1400x1050 screen resolution

Thanks.

ラベル(4)
0 件の賞賛
返信
3 返答(返信)

3,241件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Hello Alexander,

Check this out, HDMI Rotation of Android Jelly Bean


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,241件の閲覧回数
alexanderchung
Contributor II

Okay, so it does appear to work when both lvds and hmdi are specified. I was using hdmi only, and the setting had no effect.

The problem now is that even though it is portrait, it is not using the full size of the display. It has been shrunk down and centered on the hdmi display. Basically it's black on the top and bottom, with a small display frame in the middle. The lvds display is in still landscape.

Any help would be greatly appreciated.

Thanks,

Alex

0 件の賞賛
返信

3,241件の閲覧回数
alexanderchung
Contributor II

I tried that, but it doesn't appear to have any effect.

0 件の賞賛
返信