i used imx6qdl-sabreauto.dtsi
kernel 4.9.11
I connected a parallel camera to ipu1_csi0 and ipu2_csi1.
ipu1_csi0 camera is perfect run.
but ipu2_csi1 camera does not run the same way.
v4l2_cap_0 {
compatible = "fsl,imx6q-v4l2-capture";
ipu_id = <0>;
csi_id = <0>;
mclk_source = <0>;
status = "okay";
};
v4l2_cap_1 {
compatible = "fsl,imx6q-v4l2-capture";
ipu_id = <1>;
csi_id = <1>;
mclk_source = <0>;
status = "okay";
};
v4l2_out {
compatible = "fsl,mxc_v4l2_output";
status = "okay";
};
ov5642: ov5642@21 {
compatible = "daycam,ov5642";
reg = <0x21>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_ipu1_1>;
clocks = <&clks IMX6QDL_CLK_CKO>;
clock-names = "csi_mclk";
DOVDD-supply = <®_3p3v>; /* 3.3v, enabled via 2.8 VGEN6 */
AVDD-supply = <®_3p3v>; /* 1.8v */
DVDD-supply = <®_3p3v>; /* 1.8v */
PVDD-supply = <®_3p3v>; /* 1.8v */
//pwn-gpios = <&max7310_b 2 0>;
csi_id = <0>;
mclk = <24000000>;
mclk_source = <0>;
cvbs = <1>;
};
ov5642A: ov5642A@22 {
compatible = "ncam,ov5642A";
reg = <0x22>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_ipu2_1>;
clocks = <&clks IMX6QDL_CLK_CKO>;
clock-names = "csi_mclk";
DOVDD-supply = <®_3p3v>; /* 3.3v, enabled via 2.8 VGEN6 */
AVDD-supply = <®_3p3v>; /* 1.8v */
DVDD-supply = <®_3p3v>; /* 1.8v */
PVDD-supply = <®_3p3v>; /* 1.8v */
//pwn-gpios = <&max7310_b 2 0>;
csi_id = <1>;
mclk = <24000000>;
mclk_source = <0>;
cvbs = <1>;
};
The ov5462~ driver is used for ioctl purposes only.
It is not used for IC control purposes.
1. Is the device tree configured incorrectly?
2. Do I need to patch the ipu3 or v4l2 driver?