How do I stream my camera using RTSP in Gstreamer on SABRESD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How do I stream my camera using RTSP in Gstreamer on SABRESD

2,615 Views
mehdisarkeshi
Contributor I

I have searched all over the internet with no luck. I am trying to create a RTSP stream (TCP) from my SABRESD board to a Wowza server.  I have been able to create a UDP/RTP stream using the Linux guide but I can't create a RTSP stream as there is no rtspsink element. Any help is appreciated:

Labels (5)
Tags (3)
0 Kudos
Reply
3 Replies

1,968 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mehdi

one can check document ov5642-mx6qsdp-stream.pdf on

ov5642-mx6qsdp-stream.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,968 Views
mehdisarkeshi
Contributor I

Thanks Igor,

I tried this but the other end (wowza) did not recognize this as an RTSP stream. With tcpserver, I could only make it work with tcpclient sitting at the other end.

0 Kudos
Reply

1,968 Views
harshal_patel
Contributor II

Hey,

I am trying to do the exact same thing. Want to stream my camera display to WOWZA through RTSP.

Did you find a solution to your problem?

Thanks.

0 Kudos
Reply