How do I run ddr-test in U-Boot with my custom IMX6ULL Board?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How do I run ddr-test in U-Boot with my custom IMX6ULL Board?

1,012件の閲覧回数
JohnKlug
Senior Contributor I

The USB interface is not functional, as we are in development, and have no idea how to use JTAG.  SD card works.

 

I have been looking at this post:

https://community.nxp.com/t5/i-MX-Processors/About-quot-i-MX6-DDR-Stress-tester-quot/m-p/307472 

 

 

=> dcache off
=> icache off
=> fatload mmc 0:1 0x00907000 ddr-test-uboot-jtag-mx6ull.bin
** Reading file would overwrite reserved memory **

 

 

So if I use loadaddr instead:

 

 

=> printenv loadaddr 
loadaddr=0x80800000
=> fatload mmc 0:1 $loadaddr ddr-test-uboot-jtag-mx6ull.bin 
66748 bytes read in 40 ms (1.6 MiB/s)

=> go $loadaddr
## Starting application at 0x80800000 ...
data abort
pc : [<00907404>]          lr : [<9ff5132f>]
reloc pc : [<e81bb404>]    lr : [<8780532f>]
sp : 9ef43b78  ip : 00000000     fp : 00000002
r10: 9ef56768  r9 : 9ef49ed8     r8 : 9ffd5324
r7 : 9ff64cd1  r6 : 00000002     r5 : 80800000  r4 : 9ef5676c
r3 : 80800000  r2 : 9ef5676c     r1 : 9ef5676c  r0 : 00000001
Flags: nzCv  IRQs off  FIQs off  Mode SVC_32
Code: 00000000 00000000 00000000 402000d1 (87800000) 
Resetting CPU ...

resetting ...

 

0 件の賞賛
返信
1 返信

1,010件の閲覧回数
JohnKlug
Senior Contributor I

Sorry, I was on the wrong screen.  Ignore this.

0 件の賞賛
返信