How do I remove SPI chip select to clock delay in IMX6UL?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How do I remove SPI chip select to clock delay in IMX6UL?

2,275 Views
anderslorentzen
Contributor I

I keep getting a delay of 20us - 50us, when the SS is set low, to the clock and data transfer begins on the SPI ports on the imx6ul. I run a linux system on the chip with kernel version 4.9. There does not seem to be any correlation between the frequency and and the delay. Is there somewhere in the SPI driver, that I can change the parameter so this does not happen? 

See pictures for clarification, the blue is the SS pin, the yellow is CLK and purple is MOSI. 

pastedImage_2.png

pastedImage_3.png

Best regards, 

Anders

0 Kudos
Reply
2 Replies

1,889 Views
igorpadykov
NXP Employee
NXP Employee

Hi Anders

one can try patch changing "gpio" spi chip selects to spi native chip selects

kernel/git/next/linux-next.git - The linux-next integration testing tree 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,889 Views
anderslorentzen
Contributor I

Hi Igor 

The patch could not implement the 3rd change, I don't know if I missed something, I use Yocto to build the system, and just added the .diff file to my kernel.bbappend file.

I tried the 2 first changes but that did not seem to do anything to the timing from SS to CLK signal. 

Best regards, 

Anders

0 Kudos
Reply