How do I map Android GPIO to actual i.MX6 hardware pins

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How do I map Android GPIO to actual i.MX6 hardware pins

2,989 次查看
mikemandeville
Contributor II

I am putting together a rapid prototype system that is running Android on a Freescale iMX6 processor. I am trying to get the iMX6 to toggle a couple of GPIO pins, but I cannot figure out how to translate Android’s GPIO numbering to the iMX6 GPIO numbering. Android has class folders for GPIO175 and GPIO176, plus ones call GPIOCHIP128, GPIOCHIP160, etc but don’t know which GPIOs these would be on the iMX6.

标签 (2)
标记 (3)
0 项奖励
回复
1 回复

1,440 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Mike

Numbering is the same as in Linux, for example

Request the pin to be used as GPIO:

#define LED_GPIO  6*32+7  */(GPIO7_7)

For Android link below shows usage

http://android.serverbox.ch/?p=972

https://community.freescale.com/docs/DOC-1459

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复