I agree, the warning that appears seems to be unrelated as well. I have been able to verify that I can successfully run the dhcpd daemon. I do, however, have something incorrectly configured. I'm guessing my dhcpd.conf file has something wrong. My windows box issues the error upon dhcp renewal:
"An error occurred while renewing interface Ethernet : The parameter is incorrect."
However, the adapters are seeing the "foobar.com" DNS suffix
Here is my dhcpd.conf - maybe someone with better understanding can help me locate the problem.
---------------------
default-lease-time 600; # 10 minutes
max-lease-time 7200; # 2 hours
option domain-name "foobar.com";
option domain-name-servers 10.0.0.1, 10.0.0.2;
option broadcast-address 10.0.0.255;
option routers 0.0.0.254;
option subnet-mask 255.255.255.0;
subnet 10.0.0.0 netmask 255.255.255.0
{
range 10.0.0.10 10.0.0.20;
range 10.0.0.100 10.0.0.200;
}