How do I implement spread spectrum on iMX6Dual in Yocto 3.10?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How do I implement spread spectrum on iMX6Dual in Yocto 3.10?

998件の閲覧回数
davesimonson
Contributor I

I have seen the document that describes flash_headr.S, but that isn't part of Yocto.

I tried to add the code from that document into lowlevel_init.S

The result simply fails to boot.

ラベル(2)
0 件の賞賛
返信
1 返信

833件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi DAVE

please check

enable the spread spectrum 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信