How do I get a boot log?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How do I get a boot log?

2,336件の閲覧回数
jonathantaylor
Contributor II

Can someone tell me how to get a "boot log"?  I keep seeing posts where people refer to that, but I don't understand where it is coming from, and how you get a hold of a file from these MX boards when the device won't boot.  MfgTool formats the partitions, so you can't revert to a previous boot state to retrieve a file created during a failed boot (which is when you want to check a log)!  I'm missing something critical here...  Also, I see no way to adb into these board.  It seems like the MfgTool is the only way my PC can interact with it.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,180件の閲覧回数
jonathantaylor
Contributor II

Thanks Igor.  When you say it is output by MfgTools, are you referring to the mfgtool.log file?  That doesn't seem to contain anything about booting, just burning.  Is there a way to get the actual boot data from MfgTool (logcat,etc.)?  Also, how can I see the console output?

0 件の賞賛
返信

2,180件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jonathan

I meant output from console (uart).

Best regards

igor

0 件の賞賛
返信

2,180件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jonathan

boot log is messages from console during boot, also

outputted by mfg tools.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信