How do I enable CSC in Imx 6 board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How do I enable CSC in Imx 6 board

2,495 次查看
jerrald_t_g
Contributor I

I am using imx6q sabre chipset. I tried with i.MX6 CSC setting sample source code . I send commands MXCFB_SET_GAMMA,MXCFB_SET_GBL_ALPHA, I can feel the change in display,seems its working. As per the above code I sent IOCTL command MXCFB_CSC_UPDATE and no effect in display, seems code not working. then I send  IOCTL command MXCFB_SET_CLR_KEY it is also not working it went inside the file ipu_disp.c with value ipu->fg_csc_type =4. so it didnt entered the code commented with

/* Transform color key from rgb to yuv if CSC is enabled */ in file ipu_disp.c line no 728. I found this post enabling CSC.

I found the below code in line no 623 in file drivers/mxc/ipu3/ipu_disp.c.

/*

* Row is for BG: RGB2YUV YUV2RGB RGB2RGB YUV2YUV CSC_NONE
* Column is for FG: RGB2YUV YUV2RGB RGB2RGB YUV2YUV CSC_NONE
*/
static struct dp_csc_param_t dp_csc_array[CSC_NUM][CSC_NUM] = {
{{DP_COM_CONF_CSC_DEF_BOTH, &rgb2ycbcr_coeff}, {0, 0}, {0, 0}, {DP_COM_CONF_CSC_DEF_BG, &rgb2ycbcr_coeff}, {DP_COM_CONF_CSC_DEF_BG, &rgb2ycbcr_coeff} },
{{0, 0}, {DP_COM_CONF_CSC_DEF_BOTH, &ycbcr2rgb_coeff}, {DP_COM_CONF_CSC_DEF_BG, &ycbcr2rgb_coeff}, {0, 0}, {DP_COM_CONF_CSC_DEF_BG, &ycbcr2rgb_coeff} },
{{0, 0}, {DP_COM_CONF_CSC_DEF_FG, &ycbcr2rgb_coeff}, {0, 0}, {0, 0}, {0, 0} },
{{DP_COM_CONF_CSC_DEF_FG, &rgb2ycbcr_coeff}, {0, 0}, {0, 0}, {0, 0}, {0, 0} },
{{DP_COM_CONF_CSC_DEF_FG, &rgb2ycbcr_coeff}, {DP_COM_CONF_CSC_DEF_FG, &ycbcr2rgb_coeff}, {0, 0}, {0, 0}, {0, 0} }

};

please help me to  enable CSC and apply contrast for display similar to  iMX6Q display adjustment.


 

标记 (1)
0 项奖励
回复
3 回复数

1,982 次查看
AntoineP
Contributor I

Hi,

We have the exact same behaviour on our VAR-SOM-MX6 connected to an LVDS screen. MXCFB_CSC_UPDATE ioctl command doesn't seem to impact any change on the screen but MXCFB_SET_GAMMA do. How did you resolve this?

Thanks.

0 项奖励
回复

2,313 次查看
igorpadykov
NXP Employee
NXP Employee

Hi jerald

more full examples can be found on

ipu-examples release notes - v0.1 

recommended to use nxp official linux from

linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,900 次查看
lukeh
Contributor I

Hello,

Did you (or anyone else reading this) find a way to adjust the contrast on the i.MX6?

We are trying to adjust the contrast on a new display we are using but haven't had any luck. We can adjust the gamma with MXCFB_SET_GAMMA, but the contrast/color temperature doesn't change with the MXCFB_CSC_UPDATE command. We have looked through the ipu-examples but nothing has worked.

Thanks

0 项奖励
回复