How do I do I SD_VIDEO from TVE to display in the NTSC waveform

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How do I do I SD_VIDEO from TVE to display in the NTSC waveform

932 Views
daisukekitsunai
Contributor I

Hello Thank you for reading


I have been developing a custom board based on the QSB now.

And, I have to initialize the input and output of the video now.


TVE output destination is SD_VIDEO. By modifying the value of

the input clock to the chip, here is able to output to the TV color

bars.


However, the image will not be output when the input signal from

the outside of NTSC.

NTSC is that the normal waveform is observable.


How do I do I SD_VIDEO from TVE to display in the NTSC

waveform that is input to the CPU?

Can you provide instructions and a sample program?

Labels (2)
0 Kudos
Reply
1 Reply

832 Views
imxcommunitysco
Senior Contributor II

Customer also enterred a SR for this question. The SR was closed.

0 Kudos
Reply