How do I connect a different E-INK screen to the IMX50EVK daughter card?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How do I connect a different E-INK screen to the IMX50EVK daughter card?

1,077件の閲覧回数
conorross
Contributor I

I am working with the IMX50EVK and the associated daughter card MX50EBOOKDC1. This daughter card comes with a default 6 in E-ink screen which I have managed to output the linux system to. I have bought a larger E-INK screen and I want to output to this screen instead. This larger screen has a different ribbon cable. How would I be able to do this hardware wise? Are there any adapters that exist that can make this screen compatible with the daughter card?

タグ(3)
0 件の賞賛
返信
1 返信

896件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Conor

I am not aware of IMX50EVK adapters for various E-INK.

Also different Eink panel models would have different timing parameters. 

So one will have to update linux epdc driver with new timing parameter table

for that E-INK screen.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信